Hello. Is there any further suggestion on this ?
Thank you.
Hello. Is there any further suggestion on this ?
Thank you.
Dear
in datasheet of ADIS16505 on page 26 is written that
table 27, 32, 36- range is +-78.3 m/sec2 /32000 = 0.002446875 m/s and then 1LSB is 2.45mm/sec2
table 1 - Dynamic Range +-78.4m/sec2 , if range is +-78.4 m/sec2 /32000 = 0.0024500 m/s
which range and…
Dear ADI Engineers:
I met a question when I use an ADIS16505 model. I want to use its data-ready signal to interrupt my DSP. However, the signal is weird.
I do not change any default settings. I make sure the value of the MSC_CTRL register is 0x00C1 so…
Hi Experts:
Could you please provide ADIS16505-1BMLZ Theta jb value for PCB thermal simulation.
Thanks!
Hello,
Thank you for the post. In order to write to the MSC_CTRL register (or any register), the IMU must have completed its autonomous reset recovery (initialization) process. IMU initialization is required after either power up, a toggle of the rst…
Hi!Recently I purchased an ADIS16505 sensor and there was a problem reading the data.
I designed a PCB for the ADIS16505 sensor and connected it to the FPGA board(Pic 1 &Pic 2), then read sensor data through FPGA IO pins.
I follow these steps:
(1)
…It appears like this is a duplicate thread, for what was discussed in this forum. Please let me know if this was intended to ask a different question. Thank you!
https://ez.analog.com/mems/f/q-a/543604/adis16505-bias-repeatablity-for-differnt-axis
用FPGA读取ADIS16505的测量结果,操作步骤:
(1)上电
(2)等待1秒
(3)片选信号CS管脚置为0,
(4)发送0x6800(Burst模式)至DIN管脚
(5)等待160个SCLK周期后,片选信号CS置为1,然后返回第(2)布重复
结果大多数时候DOUT管脚输出都是低电平,偶尔会蹦出一些无规律的高电平,读取结果肯定不对。
将0x6800换成0x7200,按理说会收到PROD_ID 0x4079,可是结果跟发送0x6800结果一样
SCLK为1MHz时钟,占空比50%
除了以上操作步骤…
Hi,
Does the ADIS16505 have a built-in ADC? Am i right to think that the triaxial accelerometer is sampled using a 32-bit ADC since the datasheet states that the data can be outputted in a 32 bit format?