• ADIS16497 Datasheet Error, Table 1, Note 4

    PRODUCT ADIS16497
    REVISION A
    LOCATION OF ERROR Table 1, page 5 (PDF)
    DATASHEET LINK http://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16495.pdf#Page=05 
    DESCRIPTION OF ERROR

    Note 4 cites the incorrect measurement range…

  • ADIS16497 Datasheet Error; Table 1, Accelerometer Sensitivity

    PRODUCT ADIS16497
    REVISION A
    LOCATION OF ERROR Table 1, page 4 (PDF)
    DATASHEET LINK http://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16495.pdf#Page=04 
    DESCRIPTION OF ERROR

    The accelerometer sensitivity is not correct…

  • ADIS16497 - Method to determine the coordinate of ADIS16497 Signal.

    Dear Technical Support Team,

    I have trouble with determining the physical coordinate of ADIS16497. After mounting the IMU, I need to specify the physical coordinate of the IMU so that fits the signal of the sensor. However, I wonder if I can use the Edge…

  • Uncertain in burst mode ADIS16497

    Dear Analog Device, 

    When I use burst mode, I have an issue about the operation of this sensor. 

    when I used debug mode, the crc is right. But, when the software runs normaly, the crc is not correct. Can you tell me how to fix this? and what is the problem…

  • ADIS16497-3BMLZ: All iio_reg outputs and all _raw measurements always 0.

    Hi, I'm trying to read data from an ADIS16497-3BMLZ connected to an EVAL-ADISIMU1-RPIZ board which is in turn connected to a Raspberry Pi 4B running the Raspberry Pi build of Ubuntu Server 20 LTS.

    I've managed to install the drivers using modprobe…

  • ADIS16497-3BMLZ: All iio_reg outputs and all _raw measurements always 0.

    I'm re-posting this from https://ez.analog.com/mems/f/q-a/554669/adis16497-3bmlz-all-iio_reg-outputs-and-all-_raw-measurements-always-0/447031, since this seems a more appropriate forum for the question. 

    --------------------------------------------…

  • ADIS16497-2 Accelerometer offset drop while enable filter

    Hi 

      while enable accelerometer bias and filter, command sets at below:

    at page 3 , [0x0E,0x0F]  write 0x3F0A , [0x16,0x17]  write 0x5B6D, [0x18,0x19]  write 0x0005

    to enable bias and filter, I got the output: the Z-Axis(Red)  normal is -9.8M/S2, after run a…

  • RE: ADIS16497 gyro bias instability after power-on

    Hello Mark,

    I agree, the discussion of the process is outside the public forum.

    We have now obtained the required measurement stability.

    Earlier, I sent a service request and a detailed description. I am sure the history of the correspondence has been…

  • ADIS16497-2 command

    Hi,

    For ADIS16497, each register is byte accessible. If I want to configure the device, do I need to send two commands to write to both the lower byte higher byte of the register for the configuration to take effect?

    For example, if I want to toggle a…