• ADIS16495 Buffer can not be enabled

    Hello,

    I am using a Raspberry Pi with ADI-Kuiper Linux installed. I managed to install the driver for the ADIS16495 and I am also able to read data. Now I want to implement the buffer function of the module to get continuous data. I already set the enables…

  • FAQ: ADIS16495 Pin Compatibility with the ADIS16485

    Q:

    Can I connect pin 23 on the ADIS16495, to +VDD, like I could on the ADIS16485?

     

    A:

    Yes, while the current datasheet specifies this as a “do not connect” pin, this pin is not connected to anything inside of the ADIS16495 package, so it is OK to leave…

  • ADIS16495 Datasheet Error: Table 1, Accelerometer Sensitivity

    PRODUCT ADIS16495
    REVISION A
    LOCATION OF ERROR Table 1, page 4 (PDF)
    DATASHEET LINK http://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16495.pdf#Page=04 
    DESCRIPTION OF ERROR

    The units for the accelerometer sensitivity…

  • ADIS16495 Datasheet Error: Table 1, Note 4

    PRODUCT ADIS16495
    REVISION A
    LOCATION OF ERROR Table 1, page 5 (PDF)
    DATASHEET LINK http://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16495.pdf#Page=05 
    DESCRIPTION OF ERROR

    Note 4 cites the incorrect measurement range…

  • ADIS16495 SRAM Error

    Hello,

    I've been using the IMU ADIS16495-1 for a month and I've never had a problem. But 2 days ago, I tried to calibrate it by using the NULL_CONFIG register (activating the calibration for both sensor and select an average time) and the global…

  • ADIS16495

    How can I convert the output data of the table below into angles?

    The EXCEL below is the recorded data, I need formula to convert this data into angle

  • ADIS16495

    How to convert the output data of the following table into angles?

    The following EXCEL is the recorded data, I need formulas to convert this data into angles

  • ADIS16495 Decimation Rate

    Hi AD,

    I have configured the ADIS16495-1 for a decimation rate of 5. I have written 4 into the decimation register, and am expecting data at 4250/5 =850Hz. I am able to get data from required registers at this rate. But after quite a long period of continuous…

  • What is the difference between ADIS16495 and ADIS16495-1BMLZ?

    Hi, 

    What is the difference between these two products? There is a huge difference between the prices? I thought that -1BMLZ one is sending measured, sensed, and filtered data to output. Am I right?