FAQ
DATASHEETS |
ADIS16488A (Rev E, page 23, left column, second paragraph) |
URL |
http://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16488A.pdf#Page=23 |
PROBLEM DESCRIPTION |
One of the codes in the example configuration sequence… |
Q:
Where do I find information on evaluation tools for the ADIS16488A Inertial Measurement Unit (IMU)?
------------------------------------------------------------------------------------------------------------------------------------------------
A:
…TITLE | ADIS16488A Datasheet: ~CS Logic 0 Input Current Specification |
---|---|
DOCUMENT |
ADIS16488A Datasheet |
REVISION | D |
LOCATION | Table 1 - Logic 0 Input Current Specification |
DESCRIPTION |
Based on the current specifications, the Logic 0 Input Curr… |
PRODUCT
ADIS16488A | |
REVISION | C |
LOCATION OF ERROR | Figure 29, page 34 |
DATASHEET LINK | http://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16488A.pdf#page=34 |
DESCRIPTION OF ERROR |
This graphic lacks sufficient detail to understand… |
Hello All, can I interface adis16488a IMU with NI-CRIO? and I also looking at some code or driver in LabVIEW which can use for IMU data acquiring
Hi,
Im looking for a IMU unit to get roll, pitch and yaw measurements. Screening for 9 or more degrees of freedom, I could see there are 4 suggestions - ADIS 16488A, ADIS 16448, ADIS 16480 and ADIS16405, of which first 3 are of 10 degrees of freedom…
Hello,
If I didn't want to use the magnetometer on the ADIS16488A, is it possible to disable it and save the power needed to operate it?
Dear Sir,
As tittle, would you help to provide this specification (VRE) for Accelerometers & Gyroscope due to it can't be figure out in datasheet ?
Thanks