• ADIS16488

    When I install the USB connection programs for the ADIS16488 and ADIS16495 at the same time, why can't the respective software be opened at the same time to record data?

  • Additional resolution in ADIS16488

    Hello,

    I am a little confused about the  "Additional Resolution" bits of GYRO, ACCL, ... and so on. According to the definition of GYRO_LOW in the datasheet, 

    "The MSB has a weight of 0.01°/sec, and each subsequent bit has 1⁄2 the weight of the…

  • ADIS16488

    Does X_DELTANG represent the Euler angle of rotation about the x-axis? or its the roll? yaw?  pitch?

  • ADIS16488

    您好,我想请问ADIS16488能输出各个轴的方位角吗? 就是基于东北天坐标系,各个轴的输出角度?

    还有就是 在使用数据抓取的时候,需要先对ADIS16488进行校准操作吗?

  • ADIS16488

    I want to know What's the difference between Scaled Data and Unscaled Data?

  • ADIS16488

    1、Is calibration required before use?

    2、How is the X_DELTANG、 Y_DELTANG、 Z_DELTANG calculated?

    3、How to get azimuth?

  • RE: Adis16488 PROD_ID FFFF

    Thank you and please feel free to have them create screen names, if that is easier for you! I hope that you are well! 

  • ADIS16488

    你好,请问有没有人知道ADIS16488手册中的In-Run Bias Stability属性中5.1°/ hr是怎么算的,是指Allan方差中的偏见不稳定吗?以下是我计算的Allan方差图:我测的数据中Angular Random Walk为0.67,而手册中给的为0.26°/ hr-0.5,我计算的偏差不稳定为17°/ hr,请问手册中的In-Run Bias Stability如何计算并定义?我的采样频率为100Hz的。且感觉与手册中的艾伦方差图差太多,噪声也较大,请问有没有合适的解决方法…

  • ADIS16488评估板使用问题

           1. ADIS16488对应的评估板可以将角速度和加速度的信息按照某种协议经串口输出来吗?

           2. 如果不能输出来,那我们使用者该如何做才能达到这个要求?

  • ADIS16488评估板使用问题2

    亲爱的工程师您好,就是我在使用评估板过程中遇到一些问题,感谢您的解答:

    1. ADIS16488对应的评估板可以将角速度和加速度的信息按照某种协议经串口输出来吗?

    2. 如果不能输出来,那我们使用者该如何做才能达到这个要求?

    -----------------以下为引用------------------------

    刘工,目前ADIS16488是用DSP经USB接口到PC的,不是经过串口设备的,你若一定要用串口,我建议你用类似树莓派的板卡取直接读取ADIS16488的评估板数据,我们可以提供相应的驱动程序…