• ADIS16485 Nulling

    We're using a ADIS16485 in combination with a new microprocessor, as a heading reference sensor (application has been working on a different micro for years).  Most functionality is working OK; data ready line + interrupt driven SPI reads of (3) gyro…

  • FAQ: ADIS16485 Evaluation Tools (old)

    7/14/15 UPDATE

    The information is dated, but is being left online for prior users. Please see the following link for an updated version of this post, which provides the latest tools and URL links to key information

    FAQ: ADIS16485 Evaluation Tool Over…

  • Migration from ADIS16485 to ADIS16487

    Due to availability issues, a customer is interested in using the ADIS16487 in place of the ADIS16485 on an existing Printed Circuit card.  I see that the footprint and pinout are the same.

    Are there any issues which might cause problems with the migration…

  • FAQ: ADIS16495 Pin Compatibility with the ADIS16485

    Q:

    Can I connect pin 23 on the ADIS16495, to +VDD, like I could on the ADIS16485?

     

    A:

    Yes, while the current datasheet specifies this as a “do not connect” pin, this pin is not connected to anything inside of the ADIS16495 package, so it is OK to leave…

  • FAQ: ADIS16485 Center of Gravity

    THIS POST HAS LEGACY INFORMATION, WHICH WILL STAY ONLINE FOR HISTORICAL REFERENCE, BUT PLEASE CONSULT THE FOLLOWING LINK FOR NEW QUERIES ON THIS TOPIC:

    FAQ: ADIS1648x Center of Gravity

    Q:

    What is the center of gravity in the ADIS16485?

    A:

    ----------…

  • ADIS16485 Datasheet: ~CS Logic 0 Input Current Specification

    TITLE ADIS16485 Datasheet: ~CS Logic 0 Input Current Specification
    DOCUMENT

    ADIS16485 Datasheet

    REVISION F
    LOCATION Table 1 - Logic 0 Input Current Specification
    DESCRIPTION

    Based on the current specifications, the Logic 0 Input Curren…

  • FAQ: ADIS16485 Evaluation Tool Overview

    Q:

    Where do I find information on evaluation tools for the ADIS16485 Inertial Measurement Unit (IMU)?

    ----------------------------------------------------------------------------------------------------------------------------------------------

    A:

    We…

  • FAQ: External Clock for ADIS16485 on EVAL-ADIS

    Q:

    Can I drive an ADIS16485 with an external clock when using the EVAL-ADIS?

    -----------------------------------------------------------------------------------------------------------------

    A:

    Yes, you can!  The first step in this process is to determine…

  • FAQ: Synchronizing Data Capture with ADIS16485 Power-on

    Q:

    Will the EVAL-ADIS and IMU Evaluation Software enable capture of the first data sample that the ADIS16485 produces after it powers on?

    ----------------------------------------------------------------------------------------------------------------…