• Reliability and maintainability ADIS16480

    Hi,

    Exist for this product ADIS16480 an Reliability and Maintenability analysis and in particular is there the MTBF?

    Thanks

  • ADIS16480

    Hello.

    In my project I use the sensor  ADIS16480 to determine the pitch and roll during movement of a car. I need to know a value of an angle accurate to 1 degree. At the moment I use Euler Angles. The settings of the sensor   are used by default …

  • ADIS16480 DELTANG

    When I read the DELTANG registers, I seem to get the same value as the gyro registers, just scaled by 1/2460. The integration isn't happening. I had the impression these would integrate constantly, but am I mistaken and they are reset every time they…

  • ADIS16480 Datasheet Updates

    While we make every effort to provide accurate information in our datasheets, we do experience occasional mistakes and plan to start using this forum to provide early, public notification of any errors that we discover. In the ADIS16480 datasheet, revision…

  • ADIS16480 IMU PACKAGE

    1. We intend to use the IMU Package from Analog Devices (ADIS16480) in our nano-sat and use the Quaternion information from IMU to maintain the spacecraft  in an inertially fixed orientation. Alternately, we may also keep the spacecraft in the earth pointing…
  • ADIS16480 gyro issue

    I'm trying to read the gyro_x  OUT and LOW registers, but there is an awkward problem. There are continuous variable values unless the ADIS16480 has a fixed position without varying it.

    I tried also to read the pitch, roll, and yaw, The values were…

  • RE: Python code for ADIS16480/EVAL-ADIS DLL

    Hello Bivin

    I am sorry that we have not closed the loop with you, on this.  We have recently released a new evaluation tool, which comes with a much more extensive set of software development enablers: 

    https://www.analog.com/en/design-center/evaluation…

  • ADIS16480 absolute Yaw angle

    how can I get absolute yaw angle base on North, with ADIS16480. I found that after initializing 16480 in different places, different yaw angles are measured in the same direction.

  • ADIS16480 Accelerometers

    Hi,

    I've been using ADIS16485 and every thing worked well.

    When I switched to ADIS16480 I see that the x,y accelerometers are always turning to 0 is static conditions even if they expirence gravity.

    Is there a certain mode that I have to send the…

  • ADIS16480 bringup problems

    Dear All,

    I've an ADIS16480 unit and I am trying to interface with it using an Arduino UNO board. I am having some difficulties and want your help with that.

    I am using the PCB IMU1 breakout board with the module for easier interfacing.

    Setup…