FAQ
PRODUCT | ADIS16477 |
REVISION | A |
LOCATION OF ERROR | Figure 11, page 11 (PDF) |
DATASHEET LINK | http://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16475.pdf#Page=11 |
DESCRIPTION OF ERROR |
The vertical axis of Figure 11 makes reference… |
We were not having access to Data Ready signal. Please clarify if it also essential in the internal clock free running mode. To avoid the data ready signal related issues, We carried out the following tests on Friday. Some of the observations were still…
Hi.
I want to use ADIS16477 IC in my custom board which is hexagonal in shape. for best performance where should i place this component. is it must to place at exactly center of board?
ADI 专家好,我这边在调试ADIS16477时遇到几个问题需要咨询一下:
1、在ADIS477通过SPI通信与STM32F4进行通信的时候,在对ADIS16477加入了软件复位的控制寄存器,并按照手册加入了200ms的延时,但在测试数据时,静止状态下加速度会有很大的跳变在9.6-10之间。当我把这部分软件复位注释掉之后,在静态状态下可以稳定在9.81-9.83之间。请问这个是软件复位影响到了数据的传输吗?
2、第二个问题就是在对ADIS16477进行动态测试的时候,让其与ADIS16375进行对比…
hi
The nonlinearity of ADIS16477 is 0.2%(FS = 125°/sec), I have some questions about error calculation.
For example:
X axi Angular :100°/s ;
The nonlinearity error = 100°/s * 0.2% = 0.2°/s ; Is that correct?
Hi,
When reading the DIAG_STAT register back from ADIS16477 over SPI I'm getting 0x0001 back as the response. According to the datasheet bit 0 is reserved so is this a valid response? I'm getting sensible responses for product ID and firmware version…