Hi
I am considering ADIS16475-2.
I have a question about this evaluation kit (ADIS16475-2 / EVAL-ADIS-FX3Z).
Is there any support for Ubuntu (Linux OS) of the evaluation kit software driver?
I don't use Windows.
Best regards,
Yuya
Hi
I am considering ADIS16475-2.
I have a question about this evaluation kit (ADIS16475-2 / EVAL-ADIS-FX3Z).
Is there any support for Ubuntu (Linux OS) of the evaluation kit software driver?
I don't use Windows.
Best regards,
Yuya
Q:
Do you have any recommendations for using under-fill to strengthen the attachment of the ADIS16475 to a printed circuit board?
------------------------------------------------------------------------------------------------------------------------…
PRODUCT | ADIS16475 |
REVISION | A |
LOCATION OF ERROR | Figure 11, page 11 (PDF) |
DATASHEET LINK | http://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16475.pdf#Page=11 |
DESCRIPTION OF ERROR |
The vertical axis of Figure 11 makes reference… |
Hello,
I want to use my ADIS16507-1 sensor on my Raspberry Pi 4.
I compiled my kernel by adding the driver that I put in modules.
However when I load my modules, there are errors:
pi@raspberrypi:~ $ sudo modprobe adis16475 pi@raspberrypi:~ $ dmesg SPI…
It is typical in MEMS gyro for the bias to drift rapidly for some time after an initial power-on event [1,2]. In my observation of the ADIS16475-2 the gyro bias eventually stabilizes as the die temperature stabilizes.
Are there any ways to reduce how…
Hi Experts:
Could you please provide ADIS16475-1BMLZ Theta jb value for PCB thermal simulation.
Thanks!
How does varying the frequency of the SYNC input change the gyro readings?
- ADIS16475-2 configured in direct sync mode.
- Input clock configured within the 1900-2100 Hz bounds.
Is there any way for the IMU to know the *actual* frequency of the SYNC input…
As part of our development process we decided to conduct an angular
displacement test. We mount our custom board based on the ADIS16475 on a
turntable with an axis as close to vertical as possible. Physical rotations of
360 degrees are repeatedly applied…
Dear All,
I need to acquire data from IMU ADIS16475 and test a EKF quaternion from IMU against an optical system.
I would use the EVAL-ADIS-FX3 + ADIS16475-x/PCB in order to acquire the data form IMU but I need to synchronize the acquisition with the optical…