• ADIS16467 Clock Error in Scaled Sync mode

    Having an issue using the scaled sync functionality of the ADIS16567 MEMS IMU. 

    The problem is very similar to what is described in a couple related posts which don't have answers:

    https://ez.analog.com/mems/f/q-a/142639/adis16465-reading-buffer-data…

  • adis16imu4 with adis16467

    bought ADIS16IMU4 eval kit and a ADIS16467-1BMLZ imu,.

    screwed imu onto the eval board.

    I am feeding it correct data, volts, etc....but the Data out does not appear?....

    (following the proc on page 14 of datasheet to read product ID.

    I did have the…

  • ADIS16467 Data Counter Rate Problem

    Hi,

    I'm using the ADIS16467-2 IMU in my project. I have a problem about data rate.
    I'm using the IMU in internal clock mode (i.e. 2000 Hz data rate from internal clock) also reading data from a microprocessor in a 2kHz task. To check a successful…

  • ADIS16467 Max Dynamic Range

    Hi,

    in datasheet, dynamic range of adis16467-2bmlz is given as +- 500 degrees / second. However, during my readings, I saw that I could read angular speeds of about 800 degrees / second. I am also sure that these values ​​I read are correct. (I compared…

  • Calculating Group delay of ADIS16467 and ADIS16480 IMU's

    Hi,

    Is it possible to calculate the group delay accurately for the Accelerometer and Gyro outputs from the ADIS16480 and ADIS16467 datasheets? 

    Or is this figure available in some kind of format not shown in the datasheets?

    We need this information to…

  • RE: ADIS16467 SPI communication issue

    Found the same issue this last week. The problem i'm noticing (which obviously isn't the proper behavior in the data sheet) is that the samples of return data come 16 bits after when they should. What I mean is that I'm getting the correct data, but I…

  • Data Acquisition from adis16467

    Hello all,

    I have adis16467  with breakout board ADIS16IMU4/PCBZ and evaluation kit EVAL-ADIS2.

    It works well, I see the gyros and accelerators and can capture the data.

    I have two questions:

    1. how can I get access to data in some other way not through the…

  • ADIS16467 BurstMode "Low-Registers"

    Hi everyone,

    I use the ADIS16467 IMU with an external sync clock for data acquisition and read the data via spi in burst mode.

    The sync clock is between 100Hz and 1kHz from my µC.

    Is there a way to get the "Low Registers" of the gyroscope and the acceleration…

  • ADIS16467 I have question

    I see ADIS16467 datasheet. Delta velocity equation at 22pages. But this equation is not understanding.

     

    1. what is d? incremental variable int the summation formula??

    2. This delta velocity is same integral of accelerator?

    3. I want to know where I am…

  • ADIS16467-2BMLZ SPI Comms locks up

    On initial power-up, my system queries the PROD_ID register.  Upon correct response, the program sets up the IMU to use external sync pulses, and everything goes smoothly.  If the microcontroller is reset, but NOT the IMU, on the next run, this process…