In preparation for when I receive the ADIS16448 device.
When I send a DIN=0x3E00 to start burst mode. Does the ADIS16448 respond by continuously streaming data or do I need to resend the 0x3E00 every time I want the DIAG,GRYO, ACCL, etc. data?
Do you have any data related to ADIS16448 aging -change in the device parameters stability during one year and more ?(for example changes in turn on bias and scale factor).
What do the different numbers on the ADIS16448 label mean? I assume some of them are the lot/date code, and others are the serial number... maybe? Thank you.
I would like to know what connector is used on the ADIS16448 IMU. I need to know the part number of the connector so I can go get the spec sheet on it and verify the plating material/thickness that is used. Thanks!
I recently weighed 5 ADIS16448 IMUs using a calibrated digital scale with resolution of 0.1 grams. The IMUs have date codes from 2013. The results are below:
Mean = 12.62g
Std: = 0.13g
The data sheet (Rev. C) specifies 15g. Thought this might be helpful…
Check this post out, which provides some LabVIEW code and other details associated with using the ADIS16448 on a robotics platform. Enjoy!!
ADIS16448 IMU MXP Board for FIRST Robotics
Dear Analog staff, could you provide a MTBF rate prediction of the ADIS16448 device, based on the Parts Stress Analysis according to
the MIL-HDBK-217F? My application requires calculation for AUF environment, at proper cooling.
Many thanks in advance…
Q:
Can you offer more information on the sampling of sensor data in the ADIS16448?
A:
The gyroscopes, accelerometers, and temperature sensors are all sampled through a common ADC channel, which uses the following sequence to collect data samples…
Hi ADI team,
At this time the ADIS16448 is unavailable from any major distributor (farnell, DK, Mouser, RS, avnet, ...). We have an order from Farnell from mid december that is still pending and distributors tend to show delivery times around may/june…