• ADIS16445 Center of Gravity

    I also have this question and what is the Center of Gravity of the 16445 sensor.

  • ADIS16445 Gyro range

    ADIS16445 Gyro range 最大可设置为 +-250°/s,  我的问题是设备实际角速度超过250°/s, 有什么后果?

  • RE: ADIS16445 - self-test sequence

    I am glad that I wasn't too late to help you.  We now have better tools for checking for unanswered questions. Before, I just relied on the feed, which would grow quickly if I was gone for a few days....

    1. So the self-status will be in the DIAG_STAT…

  • ADIS16445 user data register read/write

    Hi:
    I am a new user of ADIS16445. I have some tedious questions need your help. Any comments would be much appreciated.
    1. after power on, I read the values stored in the data registers. The values are different from the manufacturer…
  • ADIS16445如何获得滤波前的数据?

    如上图,如何可以直接获取ADC后的数据?工厂标定和滤波中的参数如何设置?有没有详细的文档?

  • Read data from ADIS16445

    Hello Guys,

    I have an ADIS16445 connected to my STM32F407 SPI1 pins , I am trying to read XACCL_OUT & YACCL_OUT & ZACCL_OUT & XGYRO_OUT & YGYRO_OUT & ZGYRO_OUT and TEMP_OUT in normal mode described in datasheet , I already have EXTI interrupt on rising…

  • ADIS16445静止时X轴陀螺仪数据波动异常

    你好,

         我司采购了ADIS16445惯导单元,在调试的时候发现静止时,X轴的陀螺仪数据始终有0.4°/s左右的波动,而且正向波动远多于负向波动,请问这是正常的吗?如果不正常,是什么原因?怎么解决?

         谢谢!

  • Gyroscopes data SCALE for ADIS16445

    Hello Guys,

    I'm using ADIS16445 , gyroscopes in this IMU should sense and measure rotations up to ±250°/sec . this is my understanding of MEMS gyroscopes . ADIS16445 datasheet says : Triaxial digital gyroscope with digital range scaling
    ±62°/sec,…

  • ADIS16445使用前是否需要标定

    ADI工程师您好,请教一下ADIS16445在ADI出厂后是否已经标定了加速度计和陀螺?是否在转台上标定了角速度测量值?

    我们想要选用此惯性测量单元,但不知购买后是否需要用户自己去做标定校准工作?如果需要自己做有什么推荐的方法?

    感谢。

    FormerMember

  • ADIS16445 ribbon crimp connector

    Dear all.

         I am going to use the ADIS16445,but I couldn't find the proper ribbon crimp connector and ribbon cable. Could you provide suitable ribbon crimp connector and ribbon cable ?

         Thanks.

    Liu