FAQ
Q:
What can cause very large offset errors in the ADIS16405 magnetometer outputs?
---------------------------------------------------------------------------------------------------------------------
A:
One potential cause is through magnetizing internal…
PRODUCT | ADIS16405 |
REVISION | C |
LOCATION OF ERROR | Table 8, page 11 |
DATASHEET LINK | http://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16405.pdf |
DESCRIPTION OF ERROR |
The default value for the PROD_ID register is incorrect.… |
Q:
Where do I find information on evaluation tools for the ADIS16405 inertial measurement unit (IMU)?
----------------------------------------------------------------------------------------------------------------------------------------------
A:
We…
使用STM32f767与ADIS16405通信,发送读AD的命令在下一个16位时钟能正确的读到,但是读GYRO三个轴的数据是FFF3或者C005,没有出现3FFF,甚至小的情况,为什么
大家好,我的ADIS16405传感器最开始数据读取时准确正常的,后来不小心电路板不知道哪里短路,数据依然能够读取,但导致ADIS16405数据读取有问题,在没有动作的情况下读出来的数据如下:
在IMU正常时,我记得的数据GYRO基本上接近0,acc z轴为-300的样子,我测量电压发现,IMU的供电电压为4.68V,正常的时候是5V。另外,动作IMU发下数据变化却也有,但没有专门的测量工具,不知道变化趋势是否准确,这种问题请问有办法解决吗?
Thanks NevadaMark,
yesterday I created a new topic answering all your questions and providing measurement data. But it is marked as spam and so far no moderator changed this :-/
Here is the link: https://ez.analog.com/mems/f/q-a/121398/adis16460-gyroscope…