FAQ
Q:
Do you have any more details on the 1.5A surge current that the ADIS16375 draws during start-up?
A:
-----------------------------------------------------------------------------------------------------------------------------------------------
At approximately…
Q:
Where do I find information on evaluation tools for the ADIS16375 Inertial Measurement Unit (IMU)?
----------------------------------------------------------------------------------------------------------------------------------------------
A:
We…
TITLE | ADIS16375 Datasheet: ~CS Logic 0 Input Current Specification |
---|---|
DOCUMENT |
ADIS16375 Datasheet |
REVISION | C |
LOCATION | Table 1 - Logic 0 Input Current Specification |
DESCRIPTION |
Based on the current specifications, the Logic 0 Input Curren… |
Hello,
We are using the ADIS16375 IMU with a TMDSCNCD28388D, one of TI's daughter cards.
The IMU was configured and worked fine with a previous MCU, namely with the LAUNCHXL-F28379D and when we made the switch to the newer MCU everything was fine.
…We are glad that helped! Thanks again, for posting in this forum and of course, for your interest in our products!
When I statically test this device,the gyroscope and accel data random jump is very big,As shown in the picture,the gyroscope data unit is radians /s,It should not jump so much under normal circumstances
Hi everyone,
I have problem with the DEC_RATE register of ADIS16375. When I write to the register and read back, the written value of bit 9 and 8 is shift left by 1. For example: If I write 0x0102 to the DEC_RATE register, the read back value is 0x0202…
在调试ADIS16375过程中发现有一定概率(大约6个中间有一个)出现读到的数据全0的情况(包括角速率、加速度、温度及ID(实际应为16375)),特别在快速温度变化(以6℃/min降温过程中)尤其明显,不知道有谁曾经遇见此问题,是IMU自身问题还是需要特殊设置?