• FAQ: ADIS16362 Evaluation Tool Overview

    Q:

    Where do I find information on evaluation tools for the ADIS16362 inertial measurement unit (IMU)?

    ----------------------------------------------------------------------------------------------------------------------------------------------

  • ADISUSBZ with ADIS16362 Gyro Data??

    Just purchased and received an ADISUSBZ and ADIS16362 module. Utilizing IMU_6DOF (Ver 3.0) I do not see any changes on the Gyro plot display. All plot axis, for the Gyro, are enabled.  The accelerometer plot display, with similar settings, works great…

  • Questions Regarding IMU ADIS16362 and ADIS16465

    Q1: For the ADIS16465: What are the Gyroscopes and Accelerometer Initial Bias Errors?

    In the ADIS16362 Data Sheet table 1: Both values: Initial Bias Error and the In-Run Stability are given for the gyro and the accelerometer. Yet in the Data Sheet of…

  • Using NI instruments to read ADIS16362

    I am trying to use a NI compactRio to communicate with ADIS16362 by SPI.

    The code in NI website has been modified to my case.

    Analog Devices ADIS16350 High Precision Tri-Axis Inertial Sensor: SPI LabVIEW FPGA IP - National Instruments 

    I have tried…

  • Unable to read data from ADIS16362

    Hi ,

    I am new to SPI and trying to read data from the IMU.

    Can anyone share a code that is working to read data from IMU ? 

    The code I am using is

    #include <SPI.h>
    //ADIS16362 ---- Arduino Mega
    //2(SCLK)--------52(SCLK)
    //3(SS)----------53(ss)
    //4(SDO…

  • 关于ADIS16362的应用问题

    我给ADIS16362发送指令读GLOB_CMD寄存器的值,刚开始得到的字符串都是正常的,隔了几秒钟后得到的字符串就全变成了“00 22 00 00 22 00 22 00 00....”这样的形式,我想知道这是什么问题引起的?

  • ADIS16362, evaluation system of old and new

    Hi,

    It is a bit confusing that we have two different but quite similar evaluation system for ADIS devices.

    Here in case of ADIS16362, which is better to be selected ? We can see both of eva boards, ADISUSBZ and newer EVAL-ADISZ, can support this device…

  • 关于ADIS16362的SPI通信问题

    我希望通过一块飞思卡尔的16位XS128单片机的SPI模块来读取ADIS16362的数据,但是现在遇到了一点问题,怎么尝试都没有数据。。

    我的设置是:选择的是主机模式(单片机SPI为主,传感器设备为从);SPI的相位和时钟都选择的是1(CPOL=1,CPHA=1);

                         在发送数据的时候,我想通过GLOB_CMD寄存器得到所有的数据输出,因此我给SPI发送的数据指令是0x3E00

    不知道我以上的设置对不对?还有什么遗漏的吗?

  • 关于ADIS16362的数据输出问题

    如题,ADIS16362的数据输出是通过SPI接口输出的,为了能采集其输出的数据,我使用了一块SPI转串口的转换模块,所有线连接好了之后,在串口助手中没有数据显示,这是什么问题呢?

    或者如果不使用这个转换模块,我应该怎么测试或采集ADIS16362这个设备的数据输出呢?

  • RE: ADXL103/ADXL203 0 g Offset Long Term Drift

    Hello Ivan,

    I have a secondary reference, which might be helpful for you.  The ADIS16362 uses the ADXL203.  While this parameter naming convention has changed, the "Initial Bias" parameter for the Accelerometer, in the ADIS16362 datasheet incorporates…