• ADIS16360 DRIVER HELP

    I was hoping that some one could help me with making a driver for the ADIS16360. I am currently getting data, but with a lot of drift. my current set up is as mentioned an adis16360 connected to a microchip 18F45K20 and my compiler is CCS. I am polling…

  • questions about ADIS16360 Linux Driver

    I am using the Linux Driver for the ADIS16360 ( actually for the ADIS16400).  Everything works Except fot the Reset. When I do a (cat Reset). I get a (cat: reset: Permission denied). I also tried it with a sudo. Any suggestions. The second is that I am…

  • RE: example C code for SPI receive

    Hi Milos,

              You can use DMA chaining if the data is continuously available from the ADIS16360. I went through the ADIS16360 datasheet. From the datasheet I understand that the ADIS16360 DIO1 signal which indicates when data is ready. After that only the…

  • RE: IMU Sensor Selection

    Hello Jared,

    We have a wide range of IMUs that provide  a trade-space of performance, size, power and cost. The ADIS16360 is on the lowest cost/performance corner of the trade space, but it is hard for me to know what type of motion you expect to track…

  • How to make IMU sensors insusceptible to surrounding electronics?

    Hi,

    I am using two IMU sensors to perform the same tests and they are: ADIS16360 and ADIS16362.

    I attached my IMU sensor on a robot arm to take some data and the gyroscope measurements were always out of calibration after one or two trials. I took the…

  • FAQ: ADIS16364 not working on EVAL-ADIS

    Q:

    When I connect my ADIS16364 device to the EVAL-ADIS system, the gyroscopes are all pegged to 409 deg/sec and the device does not seem to be working. Any ideas?

    -----------------------------------------------------------------------------------…

  • RE: ADSP-BF537 + ADIS16350 SPI

    Hi,

    Just as I was trying to get the device datasheet, it was written in the product page: "The ADIS1635X is not recommended for new designs because ADI has announced its intent to obsolete the ADIS1635X. The recommended replacement product is the ADIS1636X…

  • RE: ADIS 16367

    Hello Sergio. 0x4200 is the burst command for the ADIS16407, not the ADIS16367.  I offered that link to help understand the more basic opportunities we see in the SPI communication at a system level. Other customers have used this option in the ADIS16367…

  • ADISUSBZ-based software bug Impacts ADIS16300 ADIS1636x ADIS1640x evaluation

    ADISUSBZ-based software bug Impacts ADIS16300 ADIS1636x ADIS1640x evaluation

     

    In the past, we have communicated via email or phone to provide support for
    your inertial sensor requirements.  I wanted to check in with you regarding
    your…
  • 问题: ADI最新中文资料(2011年3月)