• ADIS16355: Voh max

    What is Voh max for ADIS16355?

     

    The ADIS16355 actually has a +3.3V I/O bus, which is tolerant to +5V inputs. 
    No level translation will be necessary with the Blackfin.

  • RE: 有没有ADIS16355与DSP2812通信的程序?

    This question has been closed by the EZ team and is assumed answered.
  • ADIS16355 temperature calculation

    Dear Sir/Madam

    Please help me please with temperature calculation of ADIS16355.

    Real temperature according to external sensor is about 26 °C.

    XTEMP_OUT = 0x6d,

    YTEMP_OUT = 0x6e

    ZTEMP_OUT = 0x58

    From datasheet sensor parameters are Output at 25…

  • About ADIS16355 SPI-OUT

    Hello,

    I've bought ADIS-16355 and choose AT89C51ED2 to read this chip.

    I would like to connect ADSP21369 with ADIS16350 by SPI.

    Please help me, show me how it works.

    My code like follow

    /******************************************************…

  • Tag List: MEMS Inertial Sensors Tags

    The following is a list of parts this group talks about. Update as necessary.

    ad22282-a-r2, ad22290, adia16201, adis16003, adis16006, adis16203, adis16204, adis16209, adis16210, adis16223, adis16227, adis16228, adis16229, adis16240, adis16255, adis16265…

  • 2010-03-27 13:46:20     trouble getting started with SPI on BF537-STAMP

    2010-03-27 13:46:20     trouble getting started with SPI on BF537-STAMP

    Hugh Shane (UNITED STATES)

    Message: 87758   

    I am developing an application that needs to communicate over the SPI bus with an Analog Devices ADIS16355 inertial sensor. I fully understand…

  • RE: 签个到,送您好礼啦!(获奖名单已公布)

    沈阳  和平区  我做运动控制和机器人 我关注ADIS16355!

  • RE: More detailed graphs for ADIS16445

    We don't provide these types of plots anymore. Can you help us understand what information they provide, that the specification table does not?  The typical performance numbers in the specification table actually offer conservative expectations for…

  • ADIS16405应用测试_三轴姿态解算

    http://bbs.ednchina.com/uploadedn/Blog/2009/7/14/8828944f-275f-458b-8126-aa19e338dabb.JPG坛子里很少有人贴惯性导航相关算法的
    贴一个自己的3轴姿态解算方法图
    欢迎各位高人拍砖

    轴示意图:

    解算方法图:

    DIY 16XXX 惯导小板:

    三轴姿态视频,包含磁罗盘指北演示:

    http://6.cn/watch/11368073.html

    http://6.cn/p/flheAWJJqsD0mmgXL3VjRw…