• Next Generation ADIS16300?

    Q:

    I just noticed that the ADIS16300 is not recommended for new designs.  What can I use in its place?

    A:

    The ADIS16300 provide a 4DOF (degrees of freedom) function, which has 1-axis of gyroscope sensing and 3-axes of accelerometer sensing.  Since there…

  • ADISUSBZ-based software bug Impacts ADIS16300 ADIS1636x ADIS1640x evaluation

    ADISUSBZ-based software bug Impacts ADIS16300 ADIS1636x ADIS1640x evaluation

     

    In the past, we have communicated via email or phone to provide support for
    your inertial sensor requirements.  I wanted to check in with you regarding
    your evaluation…

  • ADIS16300/16305

    I want to develop car navigation system using adis16300 or adis16305.

    I think it's possible. right?

    i wanna know difference between adis16305 and adis16300.

    which one is better?

    i know adis16305 is better than adis16300, but adis16305 is expensive…

  • 你好,请问ADIS16300中的单轴陀螺仪可以垂直放置使用么?

    你好,

    根据技术手册,得知ADIS16300中只有一个Yaw方向的陀螺仪,一般情况下是将器件水平放置,可测量水平面的偏航角(Yaw)角速度。但是我目前需要测量横滚(Roll)方向上的速度,请问是否可以将器件竖立起来,从而用这个单轴陀螺仪得到某个垂面的角速度?这样子做会不会带来更大的误差?

    谢谢!

  • Tag List: MEMS Inertial Sensors Tags

    The following is a list of parts this group talks about. Update as necessary.

    ad22282-a-r2, ad22290, adia16201, adis16003, adis16006, adis16203, adis16204, adis16209, adis16210, adis16223, adis16227, adis16228, adis16229, adis16240, adis16255, adis16265…

  • Where can I get replacement for a damaged flexcable for ADIS16305 Evaluation system?

    Where can I get replacement for a damaged flexcable for ADIS16305 Evaluation
    system?

     

    The manufacturer of this flexible cable (Samtec) are no longer building this
    cable. When the ADIS16300 and ADIS16305 were first introduced in the market,

  • RE: Help on chosing the correct IMU for mobile 3D scanner?

    No,

    As I said in the previous post.

    But will these calculations be real for ADIS16305 and ADIS16300?

  • Comment on FAQ; EVAL-ADIS Software Development Tools, LabVIEW

    Hi Nevada Mark,

    1)

    Does this work well for ADIS16445 on LabVIEW-2012?

    When our customer push "Start/Cancel Stream", then this have freezed why?

    Also when he push "Read Array", then have freezed again.

    He has used SDPDrivers_2…

  • RE: How to read complete data blob of ADIS16305 using linux

    Hi Paul,

    thank you very much for the patch. The segfault is gone!

    Anyway, I don't get any data from iio_read (I should get some data output on the console from "./iio_readdev adis16300 accel_x", right?).

    With kernel 3.19.3 just nothing…