• FAQ: Continuous data sampling on ADIS16223?

    B:

    How can I get continuous data sampling on the ADIS16223?

    ---------------------------------------------------------------------------------------

    A:

    You cannot configure the ADIS16223 to provide continuous time sampling. It is designed for applications…

  • ADIS16223: Reading out sensor data continuously

    ADIS16223: I need to read out continously the X, Y, Z data, the temperature and
    supply voltage. Can I read out all register values continously.

     

    The data is not produced, continuously, so it cannot be read continuously.  The
    data is only available…

  • ADIS16223 Datasheet Errors

    DOCUMENT ADIS16223 Datasheet, Rev. 0
    http://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16223.pdf
    LOCATION Pages 15, 16 (PDF file page numbers, which are different than those at the bottom of each page)
    DESCRIPTION OF ERR…
  • RE: ADIS16223采集数值偏大问题

    This question has been closed by the EZ team and is assumed answered.
  • ADIS16223 Y and Z axis

    We are using the ADIS16223 to monitor vibration and motion of a moored watercraft. We did some testing of the accelerometer on the craft and found that the acceleration observed in the Y and Z axes is identical. I was wondering what this could be a result…

  • RE: ADIS16223 Evaluation Experience with the EVAL-ADIS

    Answered and closed. All information is listed above.

  • ADIS16223采集数据异常问题

    使用三轴加速度传感器ADIS16223时,传感器不动时数据一直跳动,最大和最小能差上百个数,在振动测试时发现测得数据又偏小。请问有没有完整的传感器驱动程序可以参考。谢谢

  • ADIS16223 Rev0 Data sheet typos?

    Are these typos? The Rev 0 Data sheet for ADIS16223 as downloaded from AD website has a couple of important typos.

    Page 14 of 20

    Alarm Indicator states "Set GLOB_CMD[4]=1 (DIN = 0xBF10)"

    The DIN should be 0xBE10 not 0xBF10 ?

     

    Page 15 of…

  • ADIS16223 alternative for real-time samplig

    Hi,
    for a previous project I bought an ADIS16223 sensor.
    However it doesn't seem suitable for my new design specifications:

    • SPI digital output
    • Measurement Range >= [-70, +70] g
    • Bandwidth >= 1 kHz
    • Real-time sample mode
    • Sensitivity …