• ADIS16210 Datasheet Error: Figure 25

    ADIS16210 Datasheet Revision B

    Figure 25, Page 18

    SOURCE: http://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16210.pdf#Page=18

    Figure 25 provides a schematic for the ADIS16210/PCBZ breakout board. The pin assignments on J1 are…

  • MTTF for ADIS16210

    What is the MTTF/MTBF for the ADIS16210?

  • ADXL345 or ADIS16210?

    What is the difference between the ADXL345 and the ADIS16210?

  • RE: Accelerometer calibration tips

    Another option to keep in mind is that ADI provides fully-calibrated devices in the following devices: ADIS16201, ADIS16203, ADIS16209 and ADIS16210. Check out this post for more information on the highest accuracy devices, ADIS16209 and ADIS16210.

  • RE: Converting Accl readings to Tilt with ADXL312

    You bet! 

    www.analog.com/ADIS16209

    www.analog.com/ADIS16210

  • RE: Re: ADIS 16210 Inclination Calculation

    Hi Peter,

    Good to hear from you. I understand where you are coming from and appreciate the push to understand operation as well as possible.  The ADIS16210 uses the atan2 function, as shown on page 12 of the ADIS16210 datasheet.  Without a better understanding…

  • RE: High Accuracy Angle Sensor

    FormerMember
    FormerMember

    Hi,

    If the relative point change, then the ADIS16209/ADIS16210 output will change too. Say, with the original reference point, the ADIS16210 output is 10deg. The reference point change 1 deg, then ADIS16210 output will change to 11 deg too. After that…

  • ADIS16209 ADIS16210- clarifications needed

     

    Dear Supporter

    need some clarifications regarding ADIS16209 and ADIS16210:

     

    "Both units ADIS16209  and ADIS 16210 state something which they call "Relative Accuracy" of +/- 0.1 deg.

    It is not clear what that means: accuracy relative…

  • ADIS16210 Pitch and Roll Calculations

    I have recently integrated the ADIS16210 into a small sensor board for measuring pitch and roll angles.  I was perplexed by the fact that my roll angle from the incline registers (depending on the gravity axis) was affected by the pitch angle.  If the pitch…

  • ADIS16210 Resolution

    Q:

    Is the resolution dependent on the sample rate settings in this product?

    A:

    Yes, it is.  The ADC inside of the ADIS16210 provides 12-bits of resolution, but a number of factors (raw sensor offset variation, sensitivity variation, etc) prevent complete…