• ADIS16203: onboard filtering

    Why are there no X-filt and Y-filt pins on ADIS16203 unlike ADIS16001?

     

    The X-filt and Y-filt pins were not included as a result of a trade-off with
    the pinout. The on-board digital filtering provides a method for reducing the
    bandwidth, which…

  • ADIS16203: Accuracy definition

    I need some clarification on accuracy specs:

    (1)I would expect that the ( relative) accuracy co-efficient is after factory
    calibrating out null and offset ? can you confirm.

    2)does this refer to relative accuracy error at 0degrees ?

    3) expect…

  • ADIS16203: Relative accuracy explanation

    What does "relative accuracy" mean? (for ADIS16203) & how measured?

     

    Relative accuracy (same as INL or Integral Nonlinearity for a data converter)
    refers to the worst case inaccuracy of the device transfer curve (usually being
    the…

  • Should pin 8 and 10 of ADIS16203 grounded

    From the datasheet, pin 8 and 10 are used for ADC/DAC auxiliary function and
    should be connected to GND for proper operation as the following shown.
    But in the document of “Inclinometer/Accelerometer Evaluation
    Board--ADIS1620x/PCB”, these…

  • RE: ADIS16203 communication problems.....

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: 关于ADIS16203传感器数据读取的问题。。。

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADIS16203 problem with clock interference

    Hello everybody,

    I'm trying to read out the Data from an ADIS16203 Inclinometer via SPI using a BeagleBone Black as Master. But the received Data I saw consists only of Zeros. Because of this I tried to look at the Signal with an Oscilloscope. What I…

  • ADIS16203 : Latency until updating data register

    Hello,

    I'd like to know the latency of ADIS16203.
    I have heard that the ADI's MEMS sensors are using sigma-delta adc usually.
    So I am guessing the ADIS16203 is same.
    Also the ADIS16203 has digital filter.

    I'd like to know the formula for computation…

  • ADIS16203 Measure stability

    Dear all,

    I'm using the ADIS16203 inclinometer and he works fine but I have some problem with the actual "measure stability". When the MEMS is fixed to the plane, the angular data oscillates on 7 - 10 measure steps (max) and it don't have a null average…