• ADIS16201: Sample rate

    How does ADIS16201 generate the sample rate?

    How accurate is the sample rate?

     

    The SMPL_PRD register sets the sample rate from 122us to 3.7ms and is based on
    an on-chip oscillator with +/-1%/@25degC +/-3% over temperature.

  • ADIS16201 not distinguish angle (tilt) from accleration

    The inclinometer works very well: if I incline the device, I can measure the
    angles correctly. But, even if I move the device in a plain PARALLEL to the
    inclinometer axis, I have some variations in the inclination data! In other
    words, if I apply…

  • ADIS16201 timing between the first and second CS cycle

    Is it really necessary to wait 33.6us min between the first and second CS cycle
    when reading via the serial interface?

     

    Yes. It's slow.

  • ADIS16201 and ADIS16209 Pins 8 and 10 Grounded - Performance Issues

    I initially used the ADIS16201 in my design. I tied pins 8 and 10 to ground.
    Later, I redesigned my system and upgraded to the ADIS16209.
    Will ADIS16209 work even if pin 8 and 10 is connected to ground or do we need
    to modify the pcb?



     

  • ADIS16201 use with FX3 Sensor Evaluation Systems board

    I have an ADIS 16201/PCB daughter board and an ADI FX3 Sensor Evaluation Systems board to test an ADIS 16201 accelerometer chip.  I do not see how to connect the two boards together with the provided 2x8 ribbon cable.  The 16201/PCB has two 2x6 connectors…

  • ADIS16201 - Output data rate? - Alternatives with wide bandwidth?

    Good afternoon everyone!

    Does anyone know what is the maximum Output Data Rate (ODR) of the sensor ADIS16201?

    Is it the same ODR when using the SPI port to access directly the digitylized measurement?

    We need a sensor with a bandwidth up to 1 kHz…

  • FAQ: Tilt Angle Window Detector

    Q:

    How can I use a tilt sensor to determine if my instrument has move clockwise or counterclockwise?

    -----------------------------------------------------------------------------------------------------------------------------------------------

    A:

    The…

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…
  • ADIS1620x Evaluation Board dimensions

    We designed a PCB and we want to mount ADIS16209 Evaluation Board on this PCB.
    Therefore the dimension of the board are important. This information is missing
    from the mechanical drawing in the ADIS1620x_PCB datasheet?

     

    We don't have any better…