• FAQ: ADIS16136 Optimization

    Q:

    Are there any tips for getting the most out of the ADIS16136?

    ----------------------------------------------------------------------------------------

    A:

    The factory-default sample rate is 1024SPS. We have seen cases where noise and stability improve…

  • FAQ: ADIS16136 Noise Behaviors

    Q:

    I have noticed that the ADIS16136 noise does not seem to follow a normal distribution. Is this expected?

    ----------------------------------------------------------------------------------------------------------------------------------------------…

  • FAQ: ADIS16136 Evaluation Tool Overview

    Q:

    Where do I find information on evaluation tools for the ADIS16136 gyroscope sensor?

    --------------------------------------------------------------------------------------------------------------------------

    A:

    We offer two different tools that support…

  • adis16136的数据输出问题

    adis16136的输出 GYRO_OUT2的格式没能理解,能否像Table 10.所示GYRO_OUT的数据格式一样给出一个或者几个典型的示例,谢谢。

  • adis16136的分辨率

    我想知道adis16136陀螺仪的分辨率是多少

  • 关于ADIS16136陀螺仪的技术咨询

    该陀螺仪输出信号是怎样,是否需要采集卡进行采集,若需要,对采集卡的要求是怎样。希望它最后测量的精度精度位0.001°是否能够实现。另外它是三轴的陀螺仪吗?

  • ADIS16136 weird behaviour

    Hi. I'm sampling the ADIS16136 gyroscope using an EVAL_ADIS with the following settings changed from the default ones:

    SMPL_PRD 000Fh

    AVG_CNT 0006h; 16sps

    DEC_RATE 0007h; 10hz

    I'm seeing a weird behaviour, the gyrsocope outputs some values with…

  • ADIS16136/PCBZ wrong connection

    Hi,

    When I try to make a wire indication on breakout board without ADIS16136 mounted I see a difference between datasheet marking and real board. Below you can see figures 23 and 5 from ADIS16136 datasheet.

    But in my ADIS16136 breakout board J1…