• FAQ: ADIS16135 Mechanical/Mounting Suggestions

    Q: Bias stability over temperature and time are important in my application, which is using the ADIS16135.  Should I consider using the same mounting suggestions that are in AN-1295, which is focused on another product family? 

    -----------------------…

  • FAQ: ADIS16135 Evaluation Tool Overview

    Q:

    Where do I find information on evaluation tools for the ADIS16135 gyroscope sensor?

    --------------------------------------------------------------------------------------------------------------------------

    A:

    We offer two different tools that support…

  • RE: Need help:stm32 communicate with ADIS16135

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADIS16135 datasheet

    Hey,

    I am trying to understand the terms In-run Bias Stability, Bias repeatability, and Sensitivity Temperature Coefficient from the datasheet: 

    http://www.analog.com/media/en/technical-documentation/data-sheets/ADIS16135.pdf#Page=08

    • I understand…
  • 关于adis16135与stm32f103的通信问题

    本人第一次接触这么高端的陀螺仪,发现有相当多的问题需要注意,来这里求助希望大神们可以帮帮我

    先说一下主要目的:希望同过读取adis16135的角速度来进行积分然后输出角度,传感器装载在一个移动底盘上。

    问题:

    1,想知道怎样确保每次读取正常的数据。adis16135和32之间用的spi通信。程序里spi的配置都根据手册上设置了,读取数据的速度都不会超过300hz(手册上说明通信速度是335hz)而且每次使用都有预热30分钟,但是读取的数据还是会出问题。现在是使用32的系统时钟写的延迟函数来控制读取间隔…

  • Need Help: Data acquisition by ADIS16135 MEMS gyroscope

    Hi,

    I need help regarding Analog Devices MEMS Gyroscope ADIS16135 and ADISUSBZ evaluation board (http://www.analog.com/en/evaluation/adisusb/eb.html)

    I am trying to calculate the noise and sensitivity of the ADIS16135 MEMS gyroscope. But, I am getting…

  • FAQ: What is the ADIS16IMU1/PCBZ?

    Q:

    What is the ADIS16IMU1/PCBZ

    -----------------------------------------------

    A:

    The ADIS16IMU1/PCBZ provides the printed circuit board and machine screw kit that used to come with the following part numbers, which are now obsolete:

    • ADIS16133/PCBZ
  • RE: ADXRS646 Self Test

    Hi Nagendran, 

    1) the ST feature performs a mechanical stimulus similar to the effect of the angular velocity. So it test the integrity of the mechanical structure of the MEMS sensor. 

    2) You are right, in the presence of a angular rate, the effect of ST…