• ADIS16080 output data rate?

    Dear all,

    May I ask a question about output data rate for ADIS16080 ?  Because datasheet has no description.

    But some Gyro MEMS datasheets describe Output Data Rate(ODR) parameter.

    Best Regards,

    Lishen

  • ADIS16080 角速度換算角度公式?

    ω = dθ/dt , 下方是tool 存出的資料及用excel換算.

     

    即使程式加 delay (10ms) 應該不影響, 只是每1sample資料需要費時約 0.0138s.

    因此, 角度值=  (Dgr/S raw data - Offset) * (時間(s)) = 當下time interval 的角度值.

     

     

    2sample, Dgr/S raw data = 11.62393, Offset = 12.01465, 時間(s)=0.0138, 因此,…

  • How to get new sensitivity for ADIS16080?

    Hi All,

    Could we provide some calibration method for user, this method give new more precision sensitivity for this ADIS16080 IC. The purpose is obtain sensitivity(initial) value for each different AIDS16080 ?   Or we just use 0.09766 Degree/Sec/LSB for…

  • Why ADIS16080 have less Log data records.

    Hi All,

    I test ADI ADIS16080 Evaluation Board and use ADI evaluation software. My purpose is that Evaluate Accuracy of Yaw angle.

    step1. Working EVB through USB cable to my Notebook. Setting ADI evaluation software as below:

        (1) select "Continous…

  • ADIS16080 Large Initial Offset

    Hi,

    I've tested ADIS16080 Evaluation Board. Self-test screen-shot you can see below. Giro is in immovable state. I use latest evaluation software version.

    Is it possible to get -27 deg/sec offset from ADIS16080? Could you please explain what does…

  • Selecting Yaw Rate Gyros

    I have a need to measure yaw rate down to 1°/s min or preferably better. I have
    been looking at your products and something like the ADIS16080 is attractive.

    I have not used anything like this before and do not consider myself able to
    interpret…

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…
  • FAQ: ADIS16209/ADIS16265 Pb-free Assembly Tips

    UPDATE ALERT!

    Please visit the following link for an updated set of assembly instructions:

    FAQ: ADIS162xx LGA Assembly Guidelines

     

    Start of older assembly instructions, for historical reference but not for present use>>

    Q:

    Do you have any tips…

  • vibration sensors - recommendation

    I have been looking for some time to source a vibration sensor that I can mount
    on motors, etc, could you please tell me if you have any versions which produce
    a 0-10v or 4-10mA output or even a intelligent sensor which can communicate via
    Modbus…

  • RE: "Resetting" AD9361 from software?

    Should be fixed now with this commit:

    drivers/iio: Fix MODULE building · analogdevicesinc/linux@9a6fef6 · GitHub

    Thanks for pointing out.

    P.S. We always accept also patches

    -Michael

    michael@mhenneri-D04:~/devel/hdl/github-linux-build/linux$ make…