Hi,
I'm trying to interface ADIS16060/PCB. I'm reading the sensor by sending 3 bytes via SPI, as written in datasheet, I concatenate 2 LSB from the first byte, whole second byte, and 4 MSB of the third byte.
The overall value seems to be logical…
Hello!
I'm trying to read out data from ADIS16060 using Stellaris LMF4120 microcontroller. Initially, hardware SPI driver was used in burst mode (3x8bit transactions at 2 MHz). After that I was switched to Bit-Banging (Software SPI) to be able to communicate…
The core sensor behaviors of noise, in-run bias stability, linear-g and gxg will all be the same, or very close. The primary difference between the ADXRS620 and ADIS16265 lie in the functional integratino, which impacts performance metrics such as sensitivity…
The ADIS16265 is a fully-calibrated, digital MEMS gyroscope that comes in a 20-pin, 11.2mm Land Grid Array package, which supports standard, Pb-free, solder-reflow assembly techniques. The most common process oversights associated with their assembly…
UPDATE ALERT!
Please visit the following link for an updated set of assembly instructions:
FAQ: ADIS162xx LGA Assembly Guidelines
Start of older assembly instructions, for historical reference but not for present use>>
Q:
Do you have any…
What is causing…