• ADIS16006 orientation

    Please can you confirm that the axes are as per the data sheet of ADIS16006.
    I am using address 1 for the Y axis and address 0 for the X axis but I appear
    to get the data reversed when compared with figure 23 of the data sheet.

     

    The datasheet is…

  • 关于ADIS16006的SPI时钟配置问题

    1.硬件上把ADIS16006SPIdsp28335SPI连接,28335的时钟配置的四种方案和ADIS16006的时序图在附件里,28335SPI是否应该选第三种(加红框)?如果不是,麻烦您解释指导;

     

    2.ADIS16006加计采样频率如果超过10k会发生采样错误,而输入的时钟频率最小是10KHz,如果CS引脚一直是低电平,是不是把时钟频率设为160KHz可能造成采样错误?

    谢谢!

  • About vibration measurement & ADIS16006

    Hello,everyone:

         we are working on a vibration measurement project for oil tank of transformer.

         Our main parameters show as following:

              Sensor type:MEMS;

              BW: 2kHz or more;

              Resolution:4mg/LSB or higher;

              FS:±5g or more;

              Noise: rms< 20mg.…

  • Dilemma: Tilt Sensor: ADIS16006 and ADIS16203???

    I am building a 2 axis tilt sensor with digital interface to host controller for which we are finalizing mems sensor. I came across two products on your website, viz. ADIS16006 and ADIS16203. One is an accelerometer whether the other is inclinometer.…

  • Is there any MTTF calculation report for the following Mems devices: ADIS16485, ADIS16445, ADIS16006?

    Hello, I need the MTTF values of the following Mems sensors:

    ADIS 16485

    ADIS 16445

    ADIS16006

    Thanks in advance!

  • ADIS16006引脚配置以及带宽与分辨率的关系

    ADIS16006引脚XFILT、YFILT电容是不是设置成一般大?且两引脚电容为零时是表示两引脚开路吗?什么都不用接吗?VCC所接电容应该设置多大比较合适?如果XFILT、YFILT两引脚电容为零此时加速度计的分辨率是多少?带宽跟分辨率的关系是什么?此外带宽对采样速度有没有影响?这些是我在看手册的疑惑,新手入门,多谢各位大神指教。

  • Tag List: MEMS Inertial Sensors Tags

    The following is a list of parts this group talks about. Update as necessary.

    ad22282-a-r2, ad22290, adia16201, adis16003, adis16006, adis16203, adis16204, adis16209, adis16210, adis16223, adis16227, adis16228, adis16229, adis16240, adis16255, adis16265…

  • TAGS LIST: Sensors & MEMS

    ADXL78
    ADXL001
    ADXL278
    ADIS16223
    ADIS16240
    ADIS16209
    ADIS16203
    ADIS16201
    ADXL193
    ADISEVAL
    ADXL1005
    ADIS16000
    ADIS16210
    ADIS16227
    ADIS16228
    ADIS16229
    ADIS16305
    ADXL1001
    ADXL1002
    ADXL1004
    ADXL103
    ADXL151
    A…
  • FAQ: ADIS16209/ADIS16265 Pb-free Assembly Tips

    UPDATE ALERT!

    Please visit the following link for an updated set of assembly instructions:

    FAQ: ADIS162xx LGA Assembly Guidelines

     

    Start of older assembly instructions, for historical reference but not for present use>>

    Q:

    Do you have any tips…