• ADGS1414D, ADG1414, ADGS5414 : Where to connect the EPAD (Vss or GND)?

    Hello, 

    I am designing a system using ADGS1414D. The datasheet says that "The exposed pad is connected internally. For increased reliability of the solder joints and maximum thermal capability, it is recommended that the exposed pad is connected to VSS…

  • Can I go below 5V on VDD in Single supply mode of ADGS1414D

    I need to switch 8 channels of analog signals with the VDD varying from 3.3V up to 15V.  Can the ADGS1414D or ADG5414 still be switched if I apply a single supply voltage of below 5V to VDD? I noticed in Figure 8 of the ADGS1414D datasheet, there is a…

  • Use of ADGS1414D for switching resisters at input of AD7616

    I am using AD7616 for data acquisition, I need to acquire 70V and 28V signals  as well as 5V analog signals. I am using a resistive dividing network to make my AD7616 channel compatible. Therefor, I need to switch the resisters to configure input range…