Absorptive options of the ADG901, ADG918, ADG936, and ADG904 switches are available. What are these and where would they be used?
Absorptive options of the ADG901, ADG918, ADG936, and ADG904 switches are available. What are these and where would they be used?
Refer LO INPUTS section at the page 6 of ADL5375 datasheet. Required LO Drive Level at ADL5375 is between -6 to +6dBm. And there are 0.9dB insertion loss at 1GHz and 3dB at 4GHz. It varies over frequency, temp,and supply voltage. Take a look at Figure…
Please excuse my late reply. Our ADG936 switch should work for you here. Its a Dual SPDT 50ohm RF switch. It is available as a reflective or an absorptive switch.
http://www.analog.com/en/rfif-components/rf-switches/adg936/products/product.html
AD8104 |
AD8105 |
AD8106 |
AD8107 |
AD8108 |
AD8109 |
AD8110 |
AD8111 |
AD8112 |
AD8113 |
AD8114 |
AD8115 |
AD8116 |
AD8117 |
AD8118 |
AD8175 |
AD8176 |
AD8177 |
AD8178 |
AD8186 |
ADV3200 |
ADV3201 |
ADV3202 |
ADV3203 |
ADV3205 |
ADV3224 |
ADV3225 |
1. 问:使用单电源工作时,ADG1612好像无法正常发射双极性信号。当信号降至地电压以下时,信号发生削波。如何避免这种情况?
答:在器件采用单电源供电时,如果源极引脚或漏极引脚上的模拟输入信号降至基板电压(Gnd)以下,则内部ESD保护二极管将开始导通。发生这种情况时,您会看到,ON通道上发生失真或削波现象,OFF通道出现电流。另外,OFF开关可能处于导通状态。为关闭该开关,必须使Vgs < Vtn ( ~ 0.7v)。最低电压被施加到栅极(这里是GND)。然而,如果S/D降至栅极电压以下…
Can you explain what insertion loss and off isolation are with respect to the ADG9xx family of switches?
With regards the ADG9xx wideband CMOS switches. What is Insertion Loss and how is it defined?
Can a dc bias greater than 0.5 V be used on the ADG9xx Wideband CMOS Switches?