• RE: HMC550A / 550AE or ADG902

    Hi Nim,

    ADG902, is a CMOS SPST switch operational from 0Hz to 4.5GHz. ADG902 is a reflective switch with a shunt switch at RF2 . Below is the link for the data sheet which has detailed information about ADG902.

    https://www.analog.com/media/en/technical…

  • ADG901/ADG902 Maximum Voltage at RFC?

    As opposed to using the ADG901 to switch a RF signal I was considering an arrangement where it only gates from the antenna through to the a receiver Rx, thus the signal power requirement is low. In such a circuit the ADG901 RFC port would be exposed to…

  • ADG902 Signal Direction

    Are RF1 and RF2 interchangable, or is a specific signal direction recommended?

  • RF SPST ADG902 switch time domain response

    Hi there,

    I intend to use the ADG902 switch for backscattering applications, with a control signal pulse of 50 MHz. The time domain response of the switch in the forward direction is shown below:

    which matches the figure in the datasheet (ignore the…

  • SPICE model of ADG902?

    Does anyone can provide the SPICE model of switch ADG902?

    Thanks,

    Danyang

  • ADG902 - Dynamic power consumption

    Hi,

    Where I can find any information about dynamic power consumption of the SPST RF switch (ADG902) ?

    I'm planning to use this switch to modulate binary data with OOK. Data rate will be 5Mbit/s and carrier about 100 MHz. To estimate consumption of this…

  • RF SPDT SW @ low frequency

    Hi all,

    Our customer will try to use the RF SPDT SW @ low frequency circuit, about 1MHz ~ 50MHz.

    They select following devices.

    ADG902

    HMC544A

    HMC194AM

    More performance data @ low frequency ~ 100MHz is available ?

    P1dB,Isolation etc.

    Best regards…

  • RE: Reflective switches

    The reflective switch is the same as the absorptive switch except the 50ohm shunt resistor is replaced by a 0ohm element.  The ADG902 (SPST), ADG919 (SPDT), ADG936R (dual SPDT), and the ADG904R (SP4T) parts are reflective switches.  A reflective switch…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • ADG918 Blocking of high amplitude signals

    I'm planning to use the ADG918 for multiplexing between two inputs. The ON path shall pass signals up to +/-0.5Vp which is nicely within the 7 dBm max. input spec. The OFF port may, however, be subjected to 20-40 ns spikes of up to +/-2Vp. My concern…