• ADG858 for USB?

    Hi,

    Could you please confirm if I can use two channels of ADG858 for USB data lines? I checked the important specifications (like On resistance, on resistance flatness, matched on resistance, bandwidth) for this device and compared with some devices…

  • ADG858: Switch state in device off state.

    Hello,

    Could someone please clarify what the truth table for ADG858 switches A and B looks like when VDD is either at 0V or not connected, and IN1 and IN2 are either Low or High?

    Thanks.

  • RE: Audio Microphone switching by ADG858BCPZ-REEL7

    Hi David,

    With regards to power consumption, the ADG858 has very low power consumption of about 5nA typical to 1uA max Idd which is roughly 16.5nW with 5.5V Vdd.

    For the noise, the ADG858 has a specified THD+N parameter equivalent to 0.06%. Is this what…

  • RE: SPDT Audio Switch 4-Channel 2:1

    Hi Pannerrajan,

    You can try ADG858 its quad SPDT/2:1 mux operates from 1.8V to 5.5V

    It has Ron <0.82 ohm over full temperature range of -40C to +85C and has low THD+ Noise = 0.06 typical.

    Please have a look at the data sheet below

    http://http…

  • What is the condition of the contact when the supply power -off

    Dear Sir/Madam,

    Maybe this is FAQ.

    As for your ADG858 analog switch,

    When the supply power shut down, then what is the contact condition?

    make? brake? otherwise high-impedance,,,,,,unknown????

    Thanks Kaos

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225