Hello!
Is it OK to tie NC pin (pin #4) to ground for ADG811YRUZ and ADG812YRUZ? Is there an internal bond?
Thank you for considering my question.
Hello!
Is it OK to tie NC pin (pin #4) to ground for ADG811YRUZ and ADG812YRUZ? Is there an internal bond?
Thank you for considering my question.
The Crosstalk and Off Isolation graphs appear to be mislabeled in the datasheet since they don't match the numbers in the specification table. Off isolation is -67dB and Crosstalk is -90dB at 100kHz, but the graphs show otherwise for both.
Hi HM72,
I checked the reports about the device however, we do not have data available for the Vdd range above. The ADG821 can work at 1.8V but it hasn’t been fully characterized.
You might want to consider using ADG811, Quad x SPST switches, as an…
Hi Donald,
May I know how would you plan to use the ADG811?
Regards,
May
Dear EricC
Sorry for my late reply for your query.
Customers requirements for high speed analog switch are as following.
1. Output capacitance : Max. 10pF
2. On Resistance : 0.5ohm
3. Current : 50mA
4. Voltage : 5V or 10V
5. Leakage Current : as low…
Hi,
Unfortunately we do not have a spice model available for the ADG1611 at this time.
What supplies are you using for the ADG1611 model?If the ADG1211 model is simulated with a dual 5V supply the model will not function properly. The ADG1211 is optimized…
AD8104 |
AD8105 |
AD8106 |
AD8107 |
AD8108 |
AD8109 |
AD8110 |
AD8111 |
AD8112 |
AD8113 |
AD8114 |
AD8115 |
AD8116 |
AD8117 |
AD8118 |
AD8175 |
AD8176 |
AD8177 |
AD8178 |
AD8186 |
ADV3200 |
ADV3201 |
ADV3202 |
ADV3203 |
ADV3205 |
ADV3224 |
ADV3225 |