• Analog Signal Range and Power Supply Voltage

    Hello expert,

    I have a question on ADG802 and all these SPST switch. In the datasheet, it says the Vs should be from 0 to Vdd V. Does it mean that the maximum voltage can be controlled by this switch is below Vdd which is around 5V?

    Or I could apply…

  • RE: How fast can ADG4612 can turn on and off

    Hi Khai,

    Can I confirm what you are trying to do here.  Sounds like you want to input some kind of analog signal into the switch and then toggle the switch at 1MHz and chop it up?  The only measurement setup we have was used for the Ton/Toff results and…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • ADG801 sinks current when enabled

    Hello,

    I am currently working with the ADG801, using it to control the flow of low power at DC.  I understand my application is not RF, however, since the device I am using is a switch that can also be used in RF signal applications I figured this would…

  • ADI芯片辨识、型号查找

    看看截图: