• RE: ADG801 sinks current when enabled

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADG801 ERROR(ORPSIM-15159): RON or ROFF greater than 1/GMIN for VSWITCH model X_U13.VON.

    Tried basic simulation of ADG801 ( spice model downloaded from AD site)

    in PSpice, cadence 17.2, got : ERROR(ORPSIM-15159): RON or ROFF greater than 1/GMIN for VSWITCH model X_U13.VON

    Could you help with this please

    Sebastian

  • ADG801_parallel multiple switch to reduce Ron

    We are reviewing ADG801 analog switch for one of our DCS project.
    Can ADG801 tie in parallel to make Ron half of the specification in datasheet?

     

    Yes It is possible to tie multiple switches in parallel to reduce the Ron
  • Can I use ADG801to switch DC bias of Gain block?

    Hi,

    I am designing a RF transmitter/ receiver system. While in receive mode (which is default mode) all the RF devices (amplifiers) of the transmitter chain need to be in off state. They will be switched ON only when in transmit mode.

    Generally I use…

  • ADG801_多开关并联以降低Ron

    我们正在为一个DCS项目评估ADG801模拟开关。

    是否可以将多个ADG801并联以使导通电阻Ron降为数据手册额定值的一半?

  • RE: Impedance of an Un-energized SPST

    Hi May,

    First of all, appreciate for all the recommendations and technical details. I am glad to have you chat with me on this.

    Let me answer your questions inset below.

    • Is there any way you can tie up the Vdd of the ADG801 to a stable 5V supply…
  • RE: ADG701/702 710L/702L as low current road switch

    Hi Ricky,

    Ok, I understand better now. The ADG701/02 could be a option as it has low Idd 1uAmax. But note its Ron is typically 2ohms comparded to 50mohms for the ADP198.  Is the reverse current protection function of the ADP198 important in this application…

  • RE: Replacement of Photorelay

    Hi Avraka,

    The requirements are different to get in a single switch.  The ADG8xx series are the lowest Ron switches we have and would satisfy the 0.5ohm requirement but if the input voltage needs to be 10V then this series is not suitable.  If 5V can be…

  • RE: Migrating from ADG1606 to ADG726

    Hello tklein,

    Here are some answers to your questions:

    1. The GND for the chip should be at 0V; the signal voltage should not go below the chip GND.
    2. Both pins are used to supply the switching components and digital supply; VDD should be supplied to…
  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225