• ADG787: Sometimes the USB is not detected!

    Hi,

    Here is a short description of my system. I have a power management IC that notifies the MCU about presence of a USB host device (when the device is connected to computer). There is a UART to USB converter from FTDI in between of MCU and ADG787 which…

  • question about ADG787 spice model showing excessive leakage current

    In the ADG787 spice model, switch SWITCH.SMOD1 is modeled with a Roff of only 2.5 Mohm, whereas all the other switches are modeled with at least 10^11 ohm off resistance. This is resulting in an unacceptable leakage current of several uA in my application…

  • RE: ADG706 spice model

    Hello Tarzan,

    We don't have a SPICE model for the ADG706 switch yet.  The closest we have would be the ADG787.  It maybe useful for you to see the performance.

    Regards,

    Eric.


  • RE: ADG858 for USB?

    Hi Vala,

    Sorry for the late reply.

    For the ADG858, the device is not tested and intended for this application so the performance of the device is not guaranteed.

    If you are looking for a quad 2:1 mux then I suggest to use ADG774 or you may also have…

  • RE: ADG884 Threshold voltage on IN1/IN2

    What I don't understand is that the ADG884 data sheet says the threshold voltage on the logic input is 2.4V maximum, but I'm applying 2.5V and it doesn't switch - so that suggests that either the data sheet is wrong or something strange is going on.…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • ADI芯片辨识、型号查找

    看看截图: