• Other NMOS switches like ADG774A or ADG794

    Hello,

    I was wondering if Analog (incl. Maxim) offered more NMOS type switches like the ADG774A and ADG794.

    I think the purely N-type switches would be way superior to the CMOS switches in many applications that do not require the full voltage range from…

  • RE: Switch USB

    Hi,

    I would recommend the ADG774A for you application. It can mux 4 input channels to 8 output channels using one digital line. It also has a large bandwidth of 400MHz so it can pass high frequency signals like USB.

    Regards,

    Stephen

  • RE: ADG794 Synchronously Rectified Charge Injection

    Hello Dan,

    Thank you for the clarification. We think that the issue could be either charge injection or leakage, or a combination. Though it is difficult to identify which is the actual cause. In this case it is probably best to do as you suggested,…

  • ADZS-SC584-EZLITE  Support

    Dear Ken,

    thank you for all this valuable information. I have some more questions:

    1) Evaluation Board questions:

    Checking the ADZS-SC584-EZLITE I´ve seen in the schematics there are two stereo audio inputs that can be switched using a ADG774A MUX. 

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • RE: IS61LV5128AL Interfacing with ADSP21369

    Hi,

    We understand that your custom board SRAM is same as our Ezkit used SRAM part.

    We would recommend you to verify your custom board SRAM hardware connection with Ezkit schematic once.

    Please find the attached ADSP-21369 EZ-KIT Lite Schematic for your…

  • ADI芯片辨识、型号查找

    看看截图: