• RE: Multiplexer output does not match the input

    Hi Pascal,

    Would you be able to remove the ADG758 from the system and test it on it's own? That would be useful as we would be able to see if the issue is being caused by the part or the other devices in the system.

    Also in the case of the ADG508…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • higher dual voltage on ADG759

    Dear analog engineers,

    I want to use the ADG759 for muxing my sensor signals at 40MHz.

    The problem I have, is that the only voltages I have on my PCB are ±3,3V and ±5,5V dual suppllies.

    I need the low Ron resistance, so other options are not available…