• ADG738 datasheet fault

    Hi dear.

    I saw this image in ADG738 datasheet Figure 30 and it looks like that there is a some mistakes in this image. pay attention to SCLK and DIN pins. why there are connected together?

  • RE: What ADC drives ADG736

    Hello,

    Apologies for the delayed response to your query.

    The ADG738 is a Dual SPDT Switch, so it is not driving the ADC as such.

    I assume in this case it is providing a path for an stimulus signal from the DAC and a measurement path to the ADC.

    If you…

  • RE: ADG731 SPI Out

    Hi,

    A part I can recommend with an SPI out is the ADG738.

    Regards,

    Stephen

  • ad7193切换通道大概需要多久?

    按cn0287的设计,打算测量4路pt100热电阻。

    测单路时,可以得到较准确的值。

    现在想这样测量,某时刻,切换adg738的通道,设置ad7193为单次转换模式,然后读取数据寄存器值;最后关断adg738所有通道,延时一会,切换到下一路温度采集通道...

    发现,切换adg738通道后立刻读取ad7193数据寄存器,得到的值为0xFFFFFF;

    尝试在adg738切换通道后加延时,结果发现要延时为1秒左右再进行数据采集,才能得到较准确的值。

  • RE: ad7193读取数据感觉被放大了一倍

    现在改成只读取第一路数据,问题依旧。

    主循环里,SPI发送数据依次为:

    1,通过SPI写ADG738寄存器,打开ADG738通道一;

    2,通过SPI读AD7193配置寄存器,并修改读取的数据;

    3,将修改后的数据通过SPI写AD7193配置急寄存器;

    4,通过SPI写AD7193模式寄存器,开始单次转换;

    5,等待MISO变低,然后通过SPI读AD7193数据寄存器;

    依次循环...

    按以上步骤的话,每次加电,读取的通道一的ADC值,可能是正常的,也可能是被放大了一倍,并且会一直保持下去…

  • ADG731 not Daisy chainable without  Dout ?

    Hi analog Team I am happy the the 32:1 analog multiplexer of yours. Much more possibilities than the ADG738 8:1 mux.

    However ADG738 has a Dout pin that permits a Daisy chain well described in the datasheet. But how on earth didn't you use one of the…

  • RE: cn0287参考电路的疑问

    你好,我正好也在做这个项目,目前也遇到了些问题,也正在解决中。

    截图中的这段中文翻译其实是有歧义的,“开启ADG738”中的开启,在英文文档中是这样的“open”,应该是断开的意思。

    就是ADG738断开,ADG702闭合,这样运放就形成了一个电压跟随器,输出电压就是AD5201的编程电压。这个输出电压加在了Ref电阻上,也就形成了偏置电压。

    共勉。

  • RE: AD5668 support in Linux with ARM Cortex-A8

    Hi Bhaskar,

    I support the AD5668. I'm not a software engineering so the Linux code doesn't mean much to me. There are no links on the evaluation board that apply directly to VoutA (TP4) so a couple of questions/comments...

    1. LK5 should be in…

  • ADG704 : Issues with switching in long run

    Hi all,

    In one of our designs we are measuring the RTD temperature using similar design architecture as that of CN-0287.

    We have used ADG704 in place of ADG738 since we had only GPIOs to control the switch. (ADG738 requires 3 wire serial interface…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225