• RE: What ADC drives ADG736

    Hello,

    Apologies for the delayed response to your query.

    The ADG738 is a Dual SPDT Switch, so it is not driving the ADC as such.

    I assume in this case it is providing a path for an stimulus signal from the DAC and a measurement path to the ADC.

    If you…

  • (ADG736)Unused channel

    Hi !

    I have a question about ADG736.

    One of our customer want to use ADG736.

    But they want to use only one channel.

    To use this device with one channel, connecting Pin4,5,6,7 to GND(PullDown) is correct?

    I read this page so I think what I think is…

  • ADG736 S overvoltage

    The figure shows the electrical circuit of a controlled voltage divider. When resistors R1 and R3 are connected to resistor R5 (via S1A, S2A), resistors R2 and R4 are not connected. When the AC_IN voltage is 10 V, the analog signal voltage at the S1B…

  • RE: ADG736BRM I2C Application

    Hello JDavis2014,

    There shouldn't be an issue using the ADG736 as a multiplexer for I2C. You need to ensure that the signals remain within the supply range of the multiplexer and from an I2C perspective, you should be conscious of the capacitance that…

  • RE: Differential signal Power divider

    Hi Tsingyang,

    I would recommend a multiplexer, a 2:1 MUX to be specific. You can find them in this link Selection Table for All Analog Switches and Multiplexers | Parametric Search | Analog Devices. For a quick suggestion, try looking at ADG824, ADG8…

  • ADAU1761 jack detcetion

    Hello,

    I would like to detect which type of jack has been inserted and use analog switch ADG736 to connect signals properly. As you can see in picture below, in first stuation the tip is Headphone (L). When the mono mic is inserted tip is now microphone…

  • RE: Accessing I2C on ADV7282-M evaluation board

    Hi Vincent,

    It is perfectly ok to connect an external I2C master to the ADV728x evaluation board using the SDA, SCL and GND pins.

    The on-board cypress microcontroller will only send I2C commands to the ADV728x if it is programmed to do so by the DVP_EVAL…

  • RE: What is system calibration and how is it implemented on the AD779x ?

    System calibration allows the converter to compensate for external system gain and offset errors, as well as its own internal errors. Calibration is basically a conversion process on two specific input voltages (zero-scale or offset calibration, and full…

  • RE: AD719x Calibration: How is System Cal implemented?

    System calibration allows the converter to compensate for external system gain and offset errors as well as its own internal errors.

    Calibration is basically a conversion process on two specific input voltages (zero scale or offset calibration and full…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225