• RE: ADG734 schematic example

    What kind of frequency signal do you plan on inputting into the IN pin ?

    Anything in the kHz range should suffice, I think there may be issues if the IN frequency is faster then the ON time of the ADG734 i.e. 19ns ( ~ 50 M Hz). As the switch may not turn…

  • RE: Spice simulation model for ADG788 or ADG734?

    Hi!

    I am also interested in the LTSpice model for ADG734.

    Regards

  • ADG734: Usage without supplies

    I've a short question concerning the analog switch ADG734 (SPDT) :

    This analog switch should be a replacement for a relay.
    Therefore I'd like to know what happens when the supply voltage of the ADG 734
    is cut off. Does it act…
  • ADG734 in audio application

    Could you please confirm what the isolation below 30kHz is for the ADG734 (TPC
    14. Off Isolation vs. Frequency of your datasheet)?
    I am going to use the ADG734 in an audio application, where a very good off
    isolation is required in the…
  • ADG734 concerns

    This has two parts:

    1) Is it okay to leave unused analog inputs on this device floating?

    2) In the case where analog input exceeds the allowable range (i.e. Ain > Vdd + 0.3V, e.g. Vdd=2.5V, Ain= 3.0V), is it known how much current the device can sink…

  • Power sequencing in ADG734 and ADG788

    Hello,

    I've been inspecting these two multiplexer and I realized very little difference between them. One of the differences that I spotted that ADG788 requires spesific power sequencing, but in ADG734's datasheet there is no advice on power sequencing…

  • RE: SPDT Audio Switch 4-Channel 2:1

    Hi Pannerrajan,

    ADG858 is available in LFCSP package only.

    But if SOIC and TSSOP package is your requirement you can try using ADG774 which is in SOIC package or ADG734 which is in LFCSP package. Both parts are suited for audio and video switching.

  • RE: AC signal through analog switches

    Hi JayG

    If you do not want to bias it. Maybe have a think about using a dual supply Analog switch e.g. like the ADG733 or ADG734 or similar

    http://www.analog.com/static/imported-files/data_sheets/ADG733_734.pdf .

    These family can do single or dual supply…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225