• RE: ADG729 - documentation problems rev.C fig17/19

    Hi,

    I had the same question. Did you manage to resolve the issue in the end?

    Best regards,

    George

  • RE: Flammability Rating ADG729 BRU

    Hi Ian,

    My apologies but it looks like we missed this question.

    Yes I can confirm the flammability rating of the ADG729 BRUZ is UL94 V-0.

    Please let me know if you need anymore information.

    Regards,

    Kevin

  • Flammability Rating ADG729 BRU

    Could you please tell me the Flammability Rating of ADG729 BRUZ.

    I assume it is UL94 V-0 but can you please confirm?

    Regards,

    Ian

  • Can I use multiple ADG729's with same I2C address?

    Hi All,

    I was wondering if it was OK to use multiple ADG729's (ie ~3 or 4) in a design that all have the same I2C address.

    I want them to change (near) simultaneously, so I was thinking that may be an option. Does anyone have any experience with…

  • RE: Two AD5933 on the same I2C bus

    You need to use two ADG728 chips. With those you can connect up to 8 AD5933, If only up to four AD5933 would suffice it is better to use one ADG729 chip (you indicated you need only two AD5933). Here is how to wire the ADG729:

    You can connect any of…

  • RE: Multiple AD5933 on one I2C bus

    LiamR can confirm this, but I don't think you can change the I2C address with the AD5933.  The only solution I can think of is to multiplex the I2C lines.  If you need to save on the number of pins from your microcontroller you could use a multiplexer…

  • ADG 729 Grounding Recommendation

    I am using the ADG 729 to route audio signals- is there a recommended way to ground/layoutthe 729 (or any I2C/SPI controlled analog mux for that matter) as to prevent contamination of the audio signal from the I2C portion? I have digital and analog ground…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225