• ADG709: Life time

    Here is 2 questions about ADG709 :

    (CMOS, 1.8V to 5.5V/+-2.5V, 3Ohm, Low Voltage, 4-/8-Channel Multiplexers)

    1 - What is the typical expected life (nb. of switches) of MOS comutations for
    a typical application ?

    1 - What is the…
  • How to measure the leakage currents of ADG709,ADG719,ADG794

    Hi,  

    When I measured the switch-off leakage current of the ADG709, I found that the value was incorrect. The test connection diagram is shown in the figure. Why is the leakage current of the test much larger than the standard maximum value of 20nA in the…

  • Possible distortion for Data Acqusition application

    I want to use ADG709 for multiplexing the calibration resistor and the resistor for measurement with AD5933. Is there any possible conflict for using those?

    Actually, I have some problem for using both. I just want to know if using them is possible.

  • RE: [Ask] ADG709BRUZ is Halogen-Free part?

    Hi Kris,

    Yes, the ADG709 is Halogen free.  There was a material change a while back to make it Halogen free.  You can check the PCN in the sample and buy section on the product page, see below.

    Regards,

    Eric.

  • ADG409: Minimum power supply

    Will the ADG409 worked on power supply 3.3 V?

     

    I assume you mean the ADG409 (2x 4:1 mux).

    ADG409 will not work correctly with 3.3V single supply. ADG709 has the same
    function but works down to a supply of 1.8V.
  • I2C addressable capacitance-to-digital converter

    My customer would like to connect 2 devices AD7151 to the same I2C line. It
    seems this is not possible, isn’t it?
    Customer do not need more inputs, this is just for security and redundancy
    reasons, it must be two separate chips. Is this…
  • RE: Load cell signal chain

    Thanks for your help.

    First I would like to add an answer to my first question:How to choose the load cell supply voltage.

    I found a documentation but in french. So I will not give a link here. I can give the main result I found: The power dissipated…

  • getting analog switch common mode down to -0.10V

    Hi

    I need the ADG709 input to go 1/10V below ground, so ourplan is to use a diode as a shunt regulator on V- (-15V at 10KOhm bias). The V+ supply pin is at 5V. Is this a viable approach? What are the pitfalls? See attached.

    Thanks

    -Tim Starr on behalf…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225