• RE: ADG708BRUZ

    Hi Kazu,

    As mentioned, we cannot guarantee the parametric performance of the ADG708 or ADG608 as these were not tested with +/- 3.3V supply rails. Ton could go longer.

    I think ton would be shorter with the ADG708. Just to remind you of the Absolute Maximum…

  • ADA4891 Output circuit design (resistor RG design value)

    Hi,

    I am making an experimental circuit and looking at the characteristics.

    I have a question, please let me know.

    The circuit of several hundred channels is switched by the multiplexer.
    The received signal is switched by the following circuit and output…

  • ADL5304 Response Time

    Hi All,

     

    One of my customer is evaluating his prototype board which has ADG708 and ADL5304 Log Converter.

    His schematic diagram is attached.

    He has one issue with the ADL5304 for determining scan rate of photo diode sensors by ADG708.

    He made test…

  • RE: Is ADG 732 suitable for fast analogue signals?

    Hi,

    The ADG708 is a 8:1 Mux with a -3dB bandwidth of 55 MHz.

    For our full list of configurations see our online selection guide here.

    Depending on your supply range and application you could also look at the ADG1206. a 16:1 mux with a BW of 185 MHz…

  • RE: ADG1402BCPZ

    Hi May

    Sorry, +/-3.3V is incorrect. I will use a single 15V power supply (VDD=15V, VSS=0V) for ADG1402BCPZ this time.

    The data sheet shows following each spec using VDD=12V and VSS=0V and they are helpful information. However I would like to know them…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • RE: AD5933 I2C SCL Minimum Frequency

    Lunatic91 schrieb:

    prashanth443,

     

    I can't post my schematic, but I will tell you it is basically the same as Figure 4 on AN-1252, only I have two ADG708 multiplexers over the Zunknown because I am switching between several different combinations…

  • RE: AD5933 what values get returned if VIN and VOUT are open?

    Thanks for the reply Louijie,

    The calibration resistance I'm using is 1.01MOhms. As for the multiplexers, I'm using two ADG708 Multiplexers. Their datasheet says that their on resistance is typically about 2.5 Ohms, and my supply voltage is 2.85 V. …

  • RE: Need an 8-channel analog mux for weak signals (mV range)

    Hello mhtariq91,

    Typically, the flattest on resistance response of a switch is in the middle of the supply voltages. For a 1mV signal I would suggest a Multiplexer that can be powered from a dual supply, which will keep the middle of the supply range…

  • RE: AD7684 Pre-Processing-Best Methods Approach

    Regarding the ADC choice, what do you recommend? How about the AD7916?

    The "programmable" gain stage is pretty complex - an ADG708 multiplexer selecting the gain resistor in the op-amp feedback loop.

    You said: "High-order filtering should…