• RE: Using ADG707 diffpair channels for single ended signals

    Hi David,

    Apologies I misread the questions you proposed, so there was a little bit of confusion.

    You are correct, the switch pair enabled is S1A & S1B, S2A & S2B etc.

    If you want to use the ADG707 as a 8 to 1 single multiplexer, then connecting…

  • ADG707 unused inputs

    What is the correct thing to do with unused differential inputs on the ADG707 mux ?

    thanks,

  • ADG707 unused inputs

    What is the correct thing to do with unused differential inputs on the ADG707 mux ?

    thanks,

  • ADG707 offset leakage current?

    The ADG707 has an ON channel leakage spec (ID, IS ON) of +/- 1 nA max over temp.  What would be the "offset leakage", or difference in leakage, between common switch points DA and DB if they are at the same voltage?  You wouldn't expect one to…

  • ADG707/706 as demultiplexer

    The  datasheet for the ADG7070/706 says:

    "These parts can operate equally well as either multiplexers or demultiplexers"

    However I really can't see how to use them as a demultiplexer, I.E one in, many out.
    Is there any examples on how to…

  • Using ADG707 for RTD Application

    Hi,

    I want to multiplex 8 RTD sensors into a single A-to-D (e.g. AD7124). I considered the ADG707 since it has a low ΔRON.

    Do you see any problem with this solution?

    thanks

    Noam

  • Using ADG707 for RTD multiplexing

    Hi,

    I want to measure 8 RTD using a single A-to-D channel. I am considering using the ADG707 as a multiplexer since it has a very low ON Resistance Match Between Channels.

    Do you see any problem with this approach?

    Should I use calibration Technic?…

  • ADG707 ON Resistance match between any two channels vsTemp

    Hi,

    I am using the ADG707.

    What is the behaviour of  "ON Resistance match between any two channels" as a function of temperature change?

    Couldn't find it in the datasheet, is it stable?

    Thanks

    Noam

  • RE: Is there a Mux which is pin compatibile with ADG707BRUZ and without clamping diode on input pin

    Hi,

    We do not have a device that is pin for pin compatible with the ADG707 that has no clamping diodes on the input pins. An option could be to use the ADG5209F. The ADG5209F has no clamping diodes on the input and can block a DC voltage when there are…

  • RE: adg507 voltage driving

    Hi Aliakbar,

    VDD = 5V for the ADG507A is okay. However, there is no specification table for this voltage so specs cannot be guaranteed.

    If guaranteed specifications are need then the ADG707 would be a good alternative as it has a full specifications table…