• RE: Temperature and humidity of ADG704

    this happened intermittent  for our project,  no solutions

  • ADG704 family

    Hello,

    I would like to know what is the # between ADG704BRM and ADG704BRMZ? It is only peak temp is different?

    Thanks,

    Vinh Le

  • RE: is it a good idea to use analog multiplexer like ADG704 for multi channel ECG signal?

    Did you have any success multiplexing AD832 signal ? I am trying to do the same with another multiplexor....

  • RE: Clarification on ADG704 maximum reflow temperature

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADG704 not work for photo diode switching

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADG704 : Issues with switching in long run

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • adg704

    Salve.

    Nella  mia applicazione (medicale) invio 16 impulsi bipolari attraverso il ponte H agli elettrodi (50us positivo 50us negativo), agendo su adg704 e il dac 

    Il circuito è ottimizzato con un carico sugli elettodi di 1Kohm quindi correnti da + e …

  • RE: AD5700 RTS switch

    Hi ,

    If you have a look at the design files, there is a switch (ADG704) implemented in the schematic.

    Are you designing the current input circuitry or the HART transmitter?

    Cheers,

    Ivan

  • MCU control AD9513

    Hi,

    I need to control the divider OUT1 of AD9513 by means MCU,

    is it possible realize by means ADG704, as shown in the scheme?

    how best to implement can be controlled by using fewer components (to save pcb space)?


  • RE: Can I have a 4:1 Mux, at DC, frequency of operation

    Hi,

    The ADG704 is a low Ron SP4T that might be a good fit for you.  Note this is a low power part.

    Regards,

    Eric.