• What is ADG702 used for?

    What is ADG702 used for?

     

    The ADG702 is used for both RTD and thermocouple measurement.

    When processing the signal from RTD, the ADG702 would open to break the
    internal loop of AD8603. The AD8603 RTD would generate a current source…
  • Can an analog signal input of 50 MHZ be used for ADG 701/ ADG 702?

    Locate the IC that can switch analogue signal flow. Is ADG701/ ADG702 suitable?

  • RE: How fast can ADG4612 can turn on and off

    Hi Khai,

    Can I confirm what you are trying to do here.  Sounds like you want to input some kind of analog signal into the switch and then toggle the switch at 1MHz and chop it up?  The only measurement setup we have was used for the Ton/Toff results and…

  • [征文] IN118的基准源用AD的芯片,上面写着D6B,困饶我很久了 AD5312


    这个芯片(AD9833)的名字我猜的,可忽略看,如果是这个芯片,左看右看也不知是干吗呢?

  • ADI芯片辨识、型号查找

    看看截图:

  • RE: ADF4118 support

    Hello

    It is not finish today.

    I use my old Arduino test software (for ADF4110) to send the values in the latches

    for the moment, Pll is not locked.

    I have a question :

    Latches are 21 bits long, I have three solutions:

    1/ in a loop sequence, check…

  • RE: cn0287参考电路的疑问

    你好,我正好也在做这个项目,目前也遇到了些问题,也正在解决中。

    截图中的这段中文翻译其实是有歧义的,“开启ADG738”中的开启,在英文文档中是这样的“open”,应该是断开的意思。

    就是ADG738断开,ADG702闭合,这样运放就形成了一个电压跟随器,输出电压就是AD5201的编程电压。这个输出电压加在了Ref电阻上,也就形成了偏置电压。

    共勉。

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225