• ADG619

    Hello.

    I need switch signals between DAC (0-5V) and DDS generator (0-2.5V)

    Please see the scatch

    I have no idea how to connect this simple circuit in a wrong way. But as a result it seems that 2 channel work in parallel.

    I mean signal  from 's1' add to…

  • ADG619 switching spike

    Hi,

    I am using ADG619 followed by a AND Gate (NC7ST08M5X). Each time ADG619 switches, there is a spike at output of the AND gate. How can I remove the spike?

    ADG619 power: +5V. Vss grounded.

    AND Gate (NC7ST98M5X) power: +3.3V.

    1PPS_CNTRL: represents IN…

  • ADG619, ADG732 power requirement

    Hi,

    ADG619's power requirement Idd is found to be 1uA as per datasheet, can I consider the same value for power budget calculation?

    As the power requirement is comparatively low I want to confirm before power budgeting, also I kindly request to advice…

  • SPICE model for ADG619

    Hi. I am using ADG619 in my circuit. Before the final implementation I want to simulate the whole circuit using a spice simulator but I'm unable to find the spice model for ADG619. Can anybody send me a ink from where I can download it. Thanks.

  • Request to share ADG732 & ADG619 impedance value

    Hi,

    I'm planning to use ADG732 & ADG619 in my project as i could not find 1:64 Analog switch.

    1) I want to know ADG732's impedance of Sx wrt D for the selected and unselected pins, i.e, impedance on S1 - S32 with respect to D when switch S1 is…

  • RE: Switch between two TCXOs to feeding ADF4350

    Hi, lotus!

    ADG619/719/749/779  analog switch not add jitter for the TCXO reference signal.

    PSB will be carefully created only.

    Regards!

  • RE: Please help me find a fast, dual supply SPDT analog switch

    What I am trying to is generate an arbitrary one-shot pulse (variable width and variable amplitude). The amplitude is set by the DAC output which is then fed into one input of switch (ADG619). The second input of the switch is ground. Then I use a pulse…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • RE: 超声成像

     PDF

    ADI提供了相关解决方案,具体请看附件。

  • ADI芯片辨识、型号查找

    看看截图: