• RE: The spice model for Multiplexer ADG608 and ADG658  have problem in PSPICE.Not compatible?

    The ADG609 model has the same issue EE-cumulus noted above.  I see that the ADG608 model is on rev 2, updated in 2018.  The ADG609 one is still rev 1.0 from 2012.  Any chance you've to a new version of the ADG609?

  • RE: ADG608 Bandwidth

    HI Davide,

    Apologies I didn't read the title of the original post so I missed the part name.

    You are correct it is not given in the data sheet. the ADG608 is quite old and at the time the Bandwidth was not specified in the datasheet.

    The ADG1608 is…

  • ADG608 or similar for +- 3.3V dual supply ?

    Hello Everyone,

    I've got signals oscillating between +35 mV and -35 mV and I need an analogue multiplexer to select from them. Signals are below 150 Hz. Supply to the circuit is dual supply 3.3V. What analogue multiplexer should I use ? I found ADG608…

  • ADG608/609 current source application and bandwidth

    We are working on a multichannel current-source-driven system, and we want to use ADG608/609 for switching channels.

    The current level is around less than 5 mA, typical around 1-2mA, and signal frequency varies up to 50MHz.

    I wonder if ADG 608/609 suit…

  • ADG706: +/- 5V supplies

    My question is the following: is it possible the ADG706 to supply with +/-5Volt
    ??

     

    No it is not.
    Dual 2.5 volts supplies are the highest that ensure the IC meets all its
    specifications.
    At +/- 3.5 volts or more you will exceed Absolute maximum…

  • RE: ADG5206 minimum voltage requirements

    Hi M. Singh,

    For 16:1 and 8:1 muxes with voltages lower than 5 V, the muxes with the lowest charge injection you will find are the ADG658 or ADG608. Unfortunately, there is no plot for charge injection at +/-3.3 V in their datasheet.

    Yours sincerely,

  • Inquiries about the ADG609 spice model

    Hi all,

     

    I have a question about the spice model of ADG609.

     

    I downloaded the ADG609 SPICE model from the web site and imported it into LTSpice and started the simulation.

    I got an error "u1:9:rbbbm:Resistance must not be zero".

     

    There was a…

  • RE: ADG708BRUZ

    Hi Kazu,

    As mentioned, we cannot guarantee the parametric performance of the ADG708 or ADG608 as these were not tested with +/- 3.3V supply rails. Ton could go longer.

    I think ton would be shorter with the ADG708. Just to remind you of the Absolute Maximum…

  • RE: High frequency square wave as MUX address signal couses problem

    I don't think charge injection by the mux is the cause of your switching noise as 6pC into your 100nF caps would only generate 60uV. However the ADG608, like most AMUX is a brake before make multiplexer, So during the transition from one to the next channel…

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225