• RE: ADG601: Connection between D and S

    Hi, Matteo Colombo.

    I have a few questions before I can evaluate the ADG601 performance:

    1. What is the value of VBatt?
    2. What do you see at +VH when SHDN is low?
    3. May I know what is the next stage of +VH connected to? I need to know the load the ADG601…
  • RE: SPICE model for ADG619

    Hi JayeshParmar,

    There are two options that can be an alternative for your simulation:

    • Using two ADG601 spice model which has the closest specs to the ADG619 but is an SPST switch. Tying  two Drains (D) together to create an SPDT is needed. However, for…
  • ADG601: Digital input from a FET

    I'm intending to use the ADG601 switch in a new design. The switch will be
    powered from +/-5V supply rails ie. Vdd=+5,Vss=-5V. I ideally wish to drive the
    ADG601 digital input from a FET (drain) and was intending to use a high value…
  • RE: ADG3308: a solution for VCCA before VCCY?

    Hi Nick,

    I was confused with the lines "VCCIO is coming from processor board, VDD is derived on my board from VCCIO, with some delay due to overvoltage protection (about 40 msecs) and soft start, 800 msecs total." and "VDD can't be made…

  • RE: Migrating from ADG1606 to ADG726

    Hello tklein,

    Here are some answers to your questions:

    1. The GND for the chip should be at 0V; the signal voltage should not go below the chip GND.
    2. Both pins are used to supply the switching components and digital supply; VDD should be supplied to…
  • [征文] IN118的基准源用AD的芯片,上面写着D6B,困饶我很久了 AD5312


    这个芯片(AD9833)的名字我猜的,可忽略看,如果是这个芯片,左看右看也不知是干吗呢?

  • ADI芯片辨识、型号查找

    看看截图:

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225