Hello,
I am using ADG5434 in closed loop feedback applications but my switch is working as desired. Please refer the below circuit which depict how i have use the switch.
Hello,
I am using ADG5434 in closed loop feedback applications but my switch is working as desired. Please refer the below circuit which depict how i have use the switch.
Hi,
I have following doubts regarding ADG5434. Could you clarify on those?.
1. Could you share the Maximum Pulse current which can be injected into the Dx/Sx pin over period of 100us? The datasheet provides value for the same over period of 1ms.
2. What…
Hi
If Exposed pad is connected to GND when using dual power supply.
Could you explain that how it is effecting to circuit functionality / performance ?
Thank you !
Hi ,
Could you please let me know if ADG5434 & ADG1434 EPAD is connected to VSS internally .
We see that it seems not to be connected internally .
ADG1434: Exposed Pad. The exposed pad is tied to the substrate, VSS .
ADG5434:The exposed pad is connected…
Hi, is it safe to leave unsed inputs, floating, at least untill the cable is plugged in which drives them, or should they have pull down resistors.
Regards, Jonathan
Sir:
Is there pspice model for ADG5412/ADG5413 or ADG5433/ADG5434? I am designing a project and need a switch that can drive output voltage as large as 30V. I want to use these switches to do a simulation first.
Thank you !
Best wishes
Jacky 2012…
HI,
You should have a look at the ADG5434. The ADG5434 is pin for pin compatible with the ADG1434 but comes with a much wider supply range. It can operate with a single supply from 9 V up to 40 V.
If you have any other questions please let me know.
Regards…
Hello,
I've got offset voltages of 0,2V with a device containing ADG333ABNZ. Do the pin compatible newer versions like ADG1434 or ADG5434 correct this?
Best regards,
Simon Brem
Hello,
My signals come from strain gauges and have a differential voltage output (some mV) around a common mode voltage of 4V.
Theses signlas may be short-cicuited to Ubat.
ADG5434 seems to correspond perfectly to my need.
Thanks
Hi, Shubham.
Regarding device recommendations, the ADG1434 would be a great choice for a compromise between on-resistance and capacitance, as well as packing 4 SPDT switches inside. However, I see from your question in the link above that capacitance…